Skip to main content
Associate
August 10, 2026
Solved

ADC2 Calibration fails on 10% of chips in Dual Mode STM32H745

  • August 10, 2026
  • 1 reply
  • 55 views

I have seen a few other posts about ADC2 calibration issues without resolution.  I’m creating this new post to provide a resolution.

Using ADC1 and ADC2 in Dual mode on STM32H745 from CM4 running at 240 MHz.  10% of boards in production (20/200) were continuously watchdog resetting.  This was traced to the ADC2 calibration getting stuck in a loop for 5 minutes (and hardware watchdog of 4s would trip).  At 240 MHz, this timeout loop should only be 2.4s.  (It would be better to use a timer function, but this is STM ADC HAL code)

    /* Wait for calibration completion */
while (LL_ADC_IsCalibrationOnGoing(hadc->Instance) != 0UL)
{
wait_loop_index++;
if (wait_loop_index >= ADC_CALIBRATION_TIMEOUT)

I’m not sure what is going on in the H7 silicon that makes the status register read so slow or why it isn’t changing in the expected 2.4s max, but STM provided a work-around.  Change the order of initialization to remove the Dual Mode config from the .ioc - generated code in main and place it after that ADC calibration.

CM4 main.c
MX_ADC1_Init()
{
HAL_ADC_Init()
//HAL_ADCEx_MultiModeConfigChannel() // remove here ->
HAL_ADC_AnalogWDGConfig()
HAL_ADC_ConfigChannel()
}

MX_ADC2_Init()
{
HAL_ADC_Init()
HAL_ADC_ConfigChannel()
}

Then our app code starts
HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED)
HAL_ADCEx_Calibration_Start(&hadc2, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED); <- no longer getting stuck here
HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) // <- add here
HAL_ADC_Start(&hadc2)
HAL_ADCEx_MultiModeStart_DMA(&hadc1, (uint32_t *)adcResultsDMA1, 256);

 

Best answer by Saket_Om

Hello ​@Michael3368 

Thanks for sharing this case and the solution you found. 

To make this post more visible and easy to find by others who may face the same issue, I mark my reply as the solution. 

But yes, the solution is on your original post! 

1 reply

Saket_OmBest answer
ST Technical Moderator
August 12, 2026

Hello ​@Michael3368 

Thanks for sharing this case and the solution you found. 

To make this post more visible and easy to find by others who may face the same issue, I mark my reply as the solution. 

But yes, the solution is on your original post! 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om