ADC with STM32F303VC
I want read ADC of STM32F303VC then display status on three LED (If ADC>1000 LED red bright,ADC<500 LED green bright and extant LED ogrange bright) programmed code below,but i don't find error.Thanks everyone!
#include ''main.h''
__IO uint16_t AD= 0,DA=0, ADC1ConvertedVoltage = 0, calibration_value = 0;
__IO uint32_t TimingDelay = 0;
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
/////////////////////////////////////////////////////////////////////////////////////////
int main(void)
{
RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div2);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE);
/* Setup SysTick Timer for 1 µsec interrupts */
if (SysTick_Config(SystemCoreClock / 1000000))
{
/* Capture error */
while (1)
{}
}
////////////////LED///////////////////////////////////
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE, ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9| GPIO_Pin_10| GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOE, &GPIO_InitStructure);
///////////////////////ADC///////////////////////////////
/* GPIOC Periph clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
/* Configure ADC Channel2 as analog input (Pin 1 of Port A-PA1) */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 ;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOA, &GPIO_InitStructure);
ADC_StructInit(&ADC_InitStructure);
////////////////////////////////////////////////////////////////////////////////////////////////
/* Calibration procedure */
ADC_VoltageRegulatorCmd(ADC1, ENABLE);
/* Insert delay equal to 10 µs */
Delay(10);
ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single);
ADC_StartCalibration(ADC1);
while(ADC_GetCalibrationStatus(ADC1) != RESET );
calibration_value = ADC_GetCalibrationValue(ADC1);
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Clock = ADC_Clock_AsynClkMode;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_OneShot;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = 0;
ADC_CommonInit(ADC1, &ADC_CommonInitStructure);
ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Enable;
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ExternalTrigConvEvent = ADC_ExternalTrigConvEvent_0;
ADC_InitStructure.ADC_ExternalTrigEventEdge = ADC_ExternalTrigEventEdge_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_OverrunMode = ADC_OverrunMode_Disable;
ADC_InitStructure.ADC_AutoInjMode = ADC_AutoInjec_Disable;
ADC_InitStructure.ADC_NbrOfRegChannel = 1;
ADC_Init(ADC1, &ADC_InitStructure);
ADC_RegularChannelConfig(ADC1, ADC_Channel_2, 1, ADC_SampleTime_4Cycles5);
//////////////////////////////////////////////////////////////////////////////////////////////
ADC_Cmd(ADC1, ENABLE);
/* wait for ADRDY */
while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_RDY));
ADC_StartConversion(ADC1);
/* Infinite loop */
while (1)
{
/* Test EOC flag */
while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);
AD =ADC_GetConversionValue(ADC1);
DA =(AD *3300)/0xFFF;
////////////////////////////////////////////////////////////////////////////////////
while(AD>1000)
{
GPIO_SetBits(GPIOE,GPIO_Pin_9);
}
while(AD<500)
{
GPIO_SetBits(GPIOE,GPIO_Pin_11);
}
GPIO_SetBits(GPIOE,GPIO_Pin_10);
}
}
////////////////////////////////////////////////////////////////////////////////////
void Delay(__IO uint32_t nTime)
{
TimingDelay = nTime;
while(TimingDelay != 0);
}
and my project here: