Skip to main content
NEERAJ GUPTA
Associate III
August 1, 2017
Question

ADC with STEmwin Generated code

Posted on August 01, 2017 at 10:31

Dear all,

              i need to monitor ADC & display the value continuously in Text box using STEmwin Generated code. My ADC driver, handling for low threshold & high threshold value is working correctly as per testing done so far but i don't know how to integrated the ADC on STEmwin Generated code. What are the basic steps to achieve this? Please! give me the required guidance.         

    This topic has been closed for replies.

    1 reply

    NEERAJ GUPTA
    Associate III
    August 4, 2017
    Posted on August 04, 2017 at 08:50

    Nobody has replied so far, anyway i have solved my problem partially but not fully.

    Now the only problem remaining is screen is flickering when the code is written like this:

    void MainTask(void)

    {

        int temperature = 0;

        WM_HWIN hDialog;

      WM_HWIN hItem;

      //unsigned char te;

        GUI_Clear();

        WM_SetDesktopColor(GUI_BLACK);

        hDialog = GUI_CreateDialogBox(_aDialogCreate, GUI_COUNTOF(_aDialogCreate), _cbDialog, WM_HBKWIN, 0, 0);

        

      //GUI_ExecDialogBox(_aDialogCreate, GUI_COUNTOF(_aDialogCreate), _cbDialog, WM_HBKWIN, 0, 0);

        //GUI_ExecCreatedDialog(hDialog);

        while(1)

        {

         //te=temperature_handling();

         //if(te==1)

         //{

            

            temperature=tempCalculate();  

            temperature=temperature/4;

            num_to_string(temperature);    

          hItem = WM_GetDialogItem(hDialog, ID_TEXT_1);

        TEXT_SetText(hItem, (const char*) string);

                

       //}

       //if(te==0)

         //{

         // hItem = WM_GetDialogItem(hDialog, ID_TEXT_1);

       // TEXT_SetText(hItem, '         ');    

       //}        

         //GUI_Delay(250);

         GUI_Exec();     

        }

    }

    When i use function GUI_CreateDialogBox screen begins to flicker but it able to get values continuously from ADC. 

    When i use function GUI_ExecDialogBox screen gets stable but it is not able to get values continuously from ADC.

    How to achieve stable Screen with ADC values? Please! help me regarding this.