Skip to main content
IIvan.20
Associate
February 16, 2022
Question

ADC with DMA doesn't work on F401CC

  • February 16, 2022
  • 3 replies
  • 1241 views

I want to use ADC for audio conversion. I have an ADC which is triggered by timer with the freq of 8kHz. Then on EXTI the ADC-DMA channel starts. It have to transfer samples to buffer circularly and when half or full transfer complete IRQ appear, the half buffer data should be processed with codec algorythm. So DMA have to fire IRQs until another EXTI won't stop it.

The problem is that this solution worked some time ago, but now after I downloaded new versions of HAL and CMSIS drivers in CubeIDE and rebuillt the project it's not. For now, after I start ADC-DMA stream, it issues only 2 interrupts for half and for full transfer complition and no more! Also ADC doesn't work at all, there are zeros in recorded data. I used debbuger and breakpoints to figure it out. I know DMA doesn't stop on debugger suspend, but breakpoints in handler must work and they worked when I did debug in the past. The timer triggering works fine.

Here is DMA channel config in stm32f4xx_hal_msp.c:

void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 if(hadc->Instance==ADC1)
 {
 /* USER CODE BEGIN ADC1_MspInit 0 */
 
 /* USER CODE END ADC1_MspInit 0 */
 /* Peripheral clock enable */
 __HAL_RCC_ADC1_CLK_ENABLE();
 
 __HAL_RCC_GPIOB_CLK_ENABLE();
 /**ADC1 GPIO Configuration
 PB0 ------> ADC1_IN8
 */
 GPIO_InitStruct.Pin = GPIO_PIN_0;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 
 /* ADC1 DMA Init */
 /* ADC1 Init */
 hdma_adc1.Instance = DMA2_Stream0;
 hdma_adc1.Init.Channel = DMA_CHANNEL_0;
 hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
 hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
 hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
 hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
 hdma_adc1.Init.Mode = DMA_CIRCULAR;
 hdma_adc1.Init.Priority = DMA_PRIORITY_VERY_HIGH;
 hdma_adc1.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 if (HAL_DMA_Init(&hdma_adc1) != HAL_OK)
 {
 Error_Handler();
 }
 
 __HAL_LINKDMA(hadc,DMA_Handle,hdma_adc1);
 
 /* USER CODE BEGIN ADC1_MspInit 1 */
 
 /* USER CODE END ADC1_MspInit 1 */
 }
 
}

ADC, TIM and DMA inits in main.c:

static void MX_ADC1_Init(void)
{
 
 /* USER CODE BEGIN ADC1_Init 0 */
 
 /* USER CODE END ADC1_Init 0 */
 
 ADC_ChannelConfTypeDef sConfig = {0};
 
 /* USER CODE BEGIN ADC1_Init 1 */
 
 /* USER CODE END ADC1_Init 1 */
 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.ScanConvMode = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T3_TRGO;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DMAContinuousRequests = DISABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
 */
 sConfig.Channel = ADC_CHANNEL_8;
 sConfig.Rank = 1;
 sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */
 
 /* USER CODE END ADC1_Init 2 */
 
}
 
/**
 * @brief TIM3 Initialization Function
 * @param None
 * @retval None
 */
static void MX_TIM3_Init(void)
{
 
 /* USER CODE BEGIN TIM3_Init 0 */
 
 /* USER CODE END TIM3_Init 0 */
 
 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 
 /* USER CODE BEGIN TIM3_Init 1 */
 
 /* USER CODE END TIM3_Init 1 */
 htim3.Instance = TIM3;
 htim3.Init.Prescaler = 0;
 htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim3.Init.Period = 10499;
 htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim3) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM3_Init 2 */
 
 /* USER CODE END TIM3_Init 2 */
 
}

IRQ handlers in stm32f4xx_it.c:

void TIM3_IRQHandler(void)
{
 /* USER CODE BEGIN TIM3_IRQn 0 */
 
 /* USER CODE END TIM3_IRQn 0 */
 HAL_TIM_IRQHandler(&htim3);
 /* USER CODE BEGIN TIM3_IRQn 1 */
 
 /* USER CODE END TIM3_IRQn 1 */
}
 
/**
 * @brief This function handles DMA2 stream0 global interrupt.
 */
void DMA2_Stream0_IRQHandler(void)
{
 /* USER CODE BEGIN DMA2_Stream0_IRQn 0 */
 /* USER CODE END DMA2_Stream0_IRQn 0 */
 HAL_DMA_IRQHandler(&hdma_adc1);
 /* USER CODE BEGIN DMA2_Stream0_IRQn 1 */
 
 /* USER CODE END DMA2_Stream0_IRQn 1 */
}

How I start and stop it using HAL:

ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;
TIM_HandleTypeDef htim3;
 
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
	if(GPIO_Pin == GPIO_PIN_7) { 
		HAL_ADC_Start_DMA(&hadc1, (uint32_t*)&IO_Buffer[0], FRAME_SIZE*2);
	}
	else
	if(GPIO_Pin == GPIO_PIN_5) { 
		HAL_ADC_Stop_DMA(&hadc1);
	}
}
 
void HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef * hadc)
{
	EncodeBuffer1();
}
 
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef * hadc)
{
	EncodeBuffer2();
}
 
int main(void){
 HAL_Init();
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_ADC1_Init();
 MX_DMA_Init();
 MX_TIM3_Init();
 
 HAL_TIM_Base_Start_IT(&htim3);
}

As I said, this code worked. And I use Cube MX so I don't miss anything.

This topic has been closed for replies.

3 replies

TDK
February 16, 2022
"If you feel a post has answered your question, please click ""Accept as Solution""."
IIvan.20
IIvan.20Author
Associate
February 16, 2022

If you mean to write

MX_DMA_Init();
MX_ADC1_Init();

it did nothing. The first thing I tried to do actually

TDK
February 16, 2022
Yes. That is one problem with the code, even if there are others as well.
"If you feel a post has answered your question, please click ""Accept as Solution""."