Skip to main content
Jérémy Da Silva
Associate II
Aug 30, 2017 1:46 PM UTC
Solved

ADC VDDA and PA2 measurement

Posted on August 30, 2017 at 15:46

Hello Community,

I work on a STM32L151CCU6 and I need your help.

I try to measure VDDA voltage in order to calculate a voltage divider on PA2 (single mode). My two ADC configuration functions are :

void MX_ADC_Init(void)

{

  GPIO_InitTypeDef gpioInit1;

  GPIO_InitTypeDef gpioInit2;

   

    gpioInit1.Pin = PID_PIN; //PA2

    gpioInit1.Mode = GPIO_MODE_ANALOG;

    gpioInit1.Pull = GPIO_NOPULL;

    HAL_GPIO_Init(PID_PORT, &gpioInit1); PA2

    

    gpioInit2.Pin = PID_POWER_SUPPLY_PIN; //PB2

    gpioInit2.Mode = GPIO_MODE_OUTPUT_PP;

    gpioInit2.Pull = GPIO_NOPULL;

    HAL_GPIO_Init(PID_POWER_SUPPLY_PORT, &gpioInit2); //PB2

    

  __HAL_RCC_ADC1_CLK_ENABLE();

  ADC_ChannelConfTypeDef sConfig;

    /**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)

    */

  adc_identification.Instance = ADC1;

  adc_identification.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV2;

  adc_identification.Init.Resolution = ADC_RESOLUTION_12B;

  adc_identification.Init.DataAlign = ADC_DATAALIGN_RIGHT;

  adc_identification.Init.ScanConvMode = ADC_SCAN_DISABLE;

  adc_identification.Init.EOCSelection = ADC_EOC_SEQ_CONV;

  adc_identification.Init.LowPowerAutoWait = ADC_AUTOWAIT_DISABLE;

  adc_identification.Init.LowPowerAutoPowerOff = ADC_AUTOPOWEROFF_DISABLE;

  adc_identification.Init.ChannelsBank = ADC_CHANNELS_BANK_A;

  adc_identification.Init.ContinuousConvMode = DISABLE;

  adc_identification.Init.NbrOfConversion = 1;

  adc_identification.Init.DiscontinuousConvMode = DISABLE;

  adc_identification.Init.ExternalTrigConv = ADC_SOFTWARE_START;

  adc_identification.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;

  adc_identification.Init.DMAContinuousRequests = DISABLE;

  if (HAL_ADC_Init(&adc_identification) != HAL_OK)

  {

    while(1);

  }

    /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.

    */

  sConfig.Channel = ADC_CHANNEL_2;

  sConfig.Rank = 1;

  sConfig.SamplingTime = ADC_SAMPLETIME_384CYCLES;

  if (HAL_ADC_ConfigChannel(&adc_identification, &sConfig) != HAL_OK)

  {

    while(1);

  }

  ADC_Enable(&adc_identification);

}

and :

void MX_ADC_VDD_Init(void)

{

  ADC_ChannelConfTypeDef sConfig;

 

  /**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)*/

  VDD_measurement.Instance = ADC1;

  VDD_measurement.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;

  VDD_measurement.Init.Resolution = ADC_RESOLUTION_12B;

  VDD_measurement.Init.DataAlign = ADC_DATAALIGN_RIGHT;

  VDD_measurement.Init.ScanConvMode = ADC_SCAN_DISABLE;

  VDD_measurement.Init.EOCSelection = ADC_EOC_SEQ_CONV;

  VDD_measurement.Init.LowPowerAutoWait = ADC_AUTOWAIT_DISABLE;

  VDD_measurement.Init.LowPowerAutoPowerOff = ADC_AUTOPOWEROFF_DISABLE;

  VDD_measurement.Init.ChannelsBank = ADC_CHANNELS_BANK_A;

  VDD_measurement.Init.ContinuousConvMode = DISABLE;

  VDD_measurement.Init.NbrOfConversion = 1;

  VDD_measurement.Init.DiscontinuousConvMode = DISABLE;

  VDD_measurement.Init.ExternalTrigConv = ADC_SOFTWARE_START;

  VDD_measurement.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;

  VDD_measurement.Init.DMAContinuousRequests = DISABLE;

  if (HAL_ADC_Init(&VDD_measurement) != HAL_OK)

  {

    while(1);

  }

    /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.

    */

  sConfig.Channel = ADC_CHANNEL_17;

  sConfig.Rank = 1;

  sConfig.SamplingTime = ADC_SAMPLETIME_4CYCLES;

  if (HAL_ADC_ConfigChannel(&VDD_measurement, &sConfig) != HAL_OK)

  {

    while(1);

  }

  ADC_Enable(&VDD_measurement);

}

When I try to measure this two ADC channel, I find 0.

I use this function : HAL_ADC_GetValue(&VDD_measurement);

Does anyone know where is my problem?

Thanks,

Jérémy

    This topic has been closed for replies.
    Vangelis Fortounas
    Associate II
    Aug 31, 2017 8:41 AM UTC
    Posted on August 31, 2017 at 10:41

    For some reason the post is doubled.

    this is the yesterday's answer

    https://community.st.com/0D50X00009XkXLlSAN

    1 reply

    Vangelis Fortounas
    Associate II
    Aug 31, 2017 8:41 AM UTC
    Posted on August 31, 2017 at 10:41

    For some reason the post is doubled.

    this is the yesterday's answer

    https://community.st.com/0D50X00009XkXLlSAN