Skip to main content
Visitor II
December 10, 2024
Question

ADC Values Stucking Issue on STM32L552RCT6 Microcontroller

I am experiencing an issue with the STM32 microcontroller used in a Battery Management System (BMS) application.

Issue Details:

  • I am using ADC to measure Temperature using NTC and voltage.
  • When a specific GPIO pin is detected as HIGH, all ADC channel values get stuck at the same reading.
  • The issue is resolved only after resetting the microcontroller.
  • This behaviour occurs randomly and is not consistent across all boards, making it difficult to reproduce.
  • I am using FreeRTOS in the microcontroller.

Additional Information:

  • The system is running FreeRTOS.
  • I am using channels 5 to 16 on ADC1.
  • ADC configuration: Sampling time is set to 24.5 cycles, and the mode is Single-Ended.
  • A filtering circuit is connected to the GPIO to handle noise and transients.

Has anyone encountered a similar issue or could provide guidance on debugging this problem? Any advice on potential root causes or solutions would be greatly appreciated.

Thank you!

This topic has been closed for replies.