Skip to main content
Associate III
Feb 19, 2024 1:11 PM UTC
Question

ADC triggered by timer running at half of expected speed

I am using NUCLEO-F756ZG board. Previously, I tried using ADC with timer trigger and it worked perfectly. Now, I tried to log the timer's pulse with another timer's input capture. It works but the captured timestamps seemed unusually slow. So, I disabled the input capture and just ran the ADC only. Now, it seems like the ADC is only sampling at half the rate I set. The settings from CubeMX are as following:

 

HCLK = 216 MHz

TIM1 (ADC trigger)

PSC = 54 (4MHz timer), ARR = 4 (1MHz pulse), CCR1 = 2

TIM2 (time measurement)

PSC = 108 (1MHz timer), ARR = 0xffffffff (MAX)

ADC

Channel 2, Prescaler 4, Resolution 12bits, DMA continuous request enabled, EOC at end of single channel, Sampling time 3 cycles.

 

This should give the ADC a maximum 1.8 Msps speed. Timer1 should be triggering it at 1MHz rate. The ADC should be able to finish each conversion before the next trigger. So, the sampling rate should be 1 Msps. I confirmed the sampling rate previously and it was 1 Msps. Now, after trying input capture with timer, the sampling rate seems to be 500 ksps. I am using a 1000 size buffer with DMA and toggling a pin every conversion complete callback. At 1 Msps sampling rate, the pin should toggle every 1 ms. However, confirmed by oscilloscope and reading CNT of timer2, its taking 2 ms. I have been already been through most things I could try but it still persists. If I double the speed of timer1 (PSC = 27), the sampling speed becomes 1 Msps. If I let the ADC run free without timer trigger and continuous conversion enabled, it samples at 1.8 Msps. So, the problem seems to be in some kind of setting which is causing the ADC to be triggered at every two pulse instead of every pulse.

My pocket oscilloscope doesn't  handle MHz frequency well. But if I bring down timer1's PWM frequency to 10 kHz or so, I can verify that the PWM frequency is exactly as programmed but ADC sampling is still half of the trigger rate.

 

Any direction or advice on how to solve this is appreciated.

 

Below is the code in main file. It's mostly CubeMX generated code.

#include "main.h"

ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;

TIM_HandleTypeDef htim1;
TIM_HandleTypeDef htim2;

//buffer
uint32_t DMA_buffer[1000];
uint32_t start, end, dur;

void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_ADC1_Init(void);
static void MX_TIM1_Init(void);
static void MX_TIM2_Init(void);

//DMA callback
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
	end = TIM2->CNT;
	dur = end-start;
	HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_3);
}

int main(void)
{
 HAL_Init();

 SystemClock_Config();

 MX_GPIO_Init();
 MX_DMA_Init();
 MX_ADC1_Init();
 MX_TIM1_Init();
 MX_TIM2_Init();
//My code
 TIM1->CCR1 = 2;
 HAL_ADC_Start_DMA(&hadc1, &DMA_buffer[0], 1000);
 HAL_TIM_Base_Start(&htim2);
 HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
 start = TIM2->CNT;

 while (1)
 {
 }
}

void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 216;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Activate the Over-Drive mode
 */
 if (HAL_PWREx_EnableOverDrive() != HAL_OK)
 {
 Error_Handler();
 }

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
 {
 Error_Handler();
 }
}

static void MX_ADC1_Init(void)
{
 ADC_ChannelConfTypeDef sConfig = {0};

 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T1_TRGO;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
 */
 sConfig.Channel = ADC_CHANNEL_2;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

static void MX_TIM1_Init(void)
{
 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};
 TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};

 htim1.Instance = TIM1;
 htim1.Init.Prescaler = 54-1;
 htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim1.Init.Period = 4-1;
 htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim1.Init.RepetitionCounter = 0;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_ENABLE;
 sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
 sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
 if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
 sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
 sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
 sBreakDeadTimeConfig.DeadTime = 0;
 sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
 sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
 sBreakDeadTimeConfig.BreakFilter = 0;
 sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
 sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;
 sBreakDeadTimeConfig.Break2Filter = 0;
 sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
 if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
 {
 Error_Handler();
 }

 HAL_TIM_MspPostInit(&htim1);
}

static void MX_TIM2_Init(void)
{
 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};

 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 108-1;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 4294967295;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
}

static void MX_DMA_Init(void)
{
 __HAL_RCC_DMA2_CLK_ENABLE();

 HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn);
}

static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOE_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_3, GPIO_PIN_RESET);

 /*Configure GPIO pin : PC3 */
 GPIO_InitStruct.Pin = GPIO_PIN_3;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
}

Thank you very much for your time.

This topic has been closed for replies.

2 replies

ST Employee
Feb 20, 2024 10:46 AM UTC

Hello @rakib2023, 

I think this is related to ADC sampling time rather than TIM configuration, since you checked the PWM frequency. 

Please check this thread, he has the same issue as you do and it turns out to be related to DMA buffer  

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
rakib2023Author
Associate III
Feb 21, 2024 3:34 AM UTC

Hello Sarra.S,

Thank you for replying. I checked the thread you linked and I had considered the possibility. But in my case, the problem seems different. And the issue seems to be related ADC triggering rather than sampling time or timer output. I don't know if for some reason timer is sending TRGO event every two pulse but that seems unlikely. I checked with DMA disabled and ADC in interrupt mode (timer PSC=5400-1, i.e., 10kHz) and from toggling a pin every interrupt, the ADC interrupt is firing every 200 us compared to timer's 100 us apart pulses. Also, tested in DMA mode by declaring 10000 sized array but only using the first 5000 as DMA buffer along with normal DMA mode. DMA is only filling the first 5000 memories, the next 5000 are empty as expected. Checked with changing DMA data length to half-word too. All of them gives same result. So, I think it's safe to say that DMA is not the problem here but rather, ADC is behaving weirdly.

To give a brief history of the problem, previously, when I tested ADC with 1 channel and DMA, it worked as expected. Next I tried with 2 channels and learned the hard way that timer trigger starts a single conversion, not a sequence of conversion. After that I reverted to 1 channel and then this problem started. The ADC trigger is acting as if its sampling 2 channels. I checked the ADC registers at runtime and everything seems fine, only one channel active and all other bits are as expected.