Skip to main content
Spaghetto
Associate III
Jul 7, 2025 12:39 PM UTC
Solved

ADC+TIM+DMA: Sample 4ch at 1MSa/S but get a callback only after a number of acquisitions

Hello forum,
I'm (still) working on a data acquisition system based on STM32H743XIH6 MCU, I'm pushing the 16bit ADC to the limits and I'm stuck on a corner.

Let me summarize first the actual code:
1) TIM1 trigger every 1us ADC1 acquisition
2) ADC1 acquire 4 ch and move data via DMA to a ADCbuf[4] (4ch scan @1MSa/s)
3) HAL_ADC_ConvCpltCallback is called (every 1us) when 2) is complete and does some calculations on ADCbuf[4]. (After 100k executions=4x100k samples a flag is risen triggering data output on the main loop).

Long story short, It works flawlessly up to 960kHz, at 1MHz randomly the callback is called again before the previous call get completely served. As far I have understood the problem is that 3) is called with a 1MHz occurrance and, context saving\restore, demand too much time to get the system online without losing any samples. 

The solution I'm trying to follow is to relax this 1us callback timing this way:
1) TIM1 trigger every 1us ADC1 acquisition 
2) ADC1 acquire 4 ch and append data via DMA to a ADCbuf[40] 
(ADC still acquire 4ch @ 1MSa/s)
3) When 10 acquisition are completed (every 10us), something (a callback?) is called and does some calculations on a (4x)10 samples batch. (After 10k executions, 4x100k samples, a flag is risen triggering data output on the main loop).

Below follow some code, how do i reconfigure ADC\DMA in order to get this acquisition scheme?
Thanks in advance for all the precious infos,
Luca

 

TIM1 config:

Spoiler
static void MX_TIM1_Init(void)
{

 /* USER CODE BEGIN TIM1_Init 0 */

 /* USER CODE END TIM1_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};
 TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};

 /* USER CODE BEGIN TIM1_Init 1 */

 /* USER CODE END TIM1_Init 1 */
 htim1.Instance = TIM1;
 htim1.Init.Prescaler = 23;
 htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim1.Init.Period = 9;
 htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim1.Init.RepetitionCounter = 0;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
 if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 1;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
 sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
 if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
 sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
 sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
 sBreakDeadTimeConfig.DeadTime = 0;
 sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
 sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
 sBreakDeadTimeConfig.BreakFilter = 0;
 sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
 sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;
 sBreakDeadTimeConfig.Break2Filter = 0;
 sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
 if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM1_Init 2 */

 /* USER CODE END TIM1_Init 2 */
 HAL_TIM_MspPostInit(&htim1);

}

ADC config:

Spoiler
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_16B;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 4;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T1_TRGO;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
 hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
 hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
 hadc1.Init.OversamplingMode = DISABLE;
 hadc1.Init.Oversampling.Ratio = 1;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the ADC multi-mode
 */
 multimode.Mode = ADC_MODE_INDEPENDENT;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_0;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 sConfig.OffsetSignedSaturation = DISABLE;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_3;
 sConfig.Rank = ADC_REGULAR_RANK_3;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_4;
 sConfig.Rank = ADC_REGULAR_RANK_4;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

Context and Callback:

Spoiler
//Following is placed in D2 RAM as per https://community.st.com/t5/stm32-mcus/dma-is-not-working-on-stm32h7-devices/ta-p/49498
__attribute__((section(".dma_buffer"))) uint16_t 	ADCbuf[4];		//ADC to DMA buffer (4ch)
...
 //ADC Calibration
 if(HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED) != HAL_OK){
...
 //ADC Start
 if(HAL_ADC_Start_DMA(&hadc1, (uint32_t *)ADCbuf, 4) != HAL_OK){
...
 //Start TIM1 (ADC trigger\timebase: 1MSa/s per eachchannel -> 1MHz)
 if(HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1) != HAL_OK){
...
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc){ //todo: ADC callback
			//Add val^2 to sum (RMS)
			SumR[0] += (uint32_t)ADCbuf[0]*ADCbuf[0];
			SumR[1] += (uint32_t)ADCbuf[1]*ADCbuf[1];
			SumR[2] += (uint32_t)ADCbuf[2]*ADCbuf[2];
			SumR[3] += (uint32_t)ADCbuf[3]*ADCbuf[3];

		if(Index>=Astop){ //Buffer full (end of frame acquisition)

			#ifdef OVERRUN_LOCK
			if(ADCcmplt){
				HAL_TIM_PWM_Stop(&htim1, TIM_CHANNEL_1);
				Overrun=1;
			}
			#endif

			//Transfer SumR and Reset
			SumRO[0]=SumR[0];
			SumRO[1]=SumR[1];
			SumRO[2]=SumR[2];
			SumRO[3]=SumR[3];
			SumR[0] = 0;
			SumR[1] = 0;
			SumR[2] = 0;
			SumR[3] = 0;

			Index = Astart; //Reset Index
			ADCcmplt=1;
		}
		else Index++;
}

 

This topic has been closed for replies.
KnarfB
KnarfBBest answer
Super User
Jul 7, 2025 1:17 PM UTC

Don't use the ADC interrupt/callback, but the DMA. Config circular DMA which is "endless". Config Half transfer and transfer complete interrupts. In each DMA interrupt callback, process the half of the buffer that is finished while the ADC keeps filling the other half.

hth

KnarfB

5 replies

KnarfB
KnarfBBest answer
Super User
Jul 7, 2025 1:17 PM UTC

Don't use the ADC interrupt/callback, but the DMA. Config circular DMA which is "endless". Config Half transfer and transfer complete interrupts. In each DMA interrupt callback, process the half of the buffer that is finished while the ADC keeps filling the other half.

hth

KnarfB

Spaghetto
SpaghettoAuthor
Associate III
Jul 7, 2025 2:40 PM UTC

Hi @KnarfB ,
do you mean using HAL_ADC_ConvHalfCpltCallback() beside the HAL_ADC_ConvCpltCallback() (which I'm already using)? That's interesting since I didn't realized before that I could lose samples if the ADC overwrite the very first data if I'm not serving interrupt quickly (before the new sampling group 1-10).

DMA is already circular, therefore should I just do the following 4->40 and add the Half callback?

__attribute__((section(".dma_buffer"))) uint16_t 	ADCbuf[40];
...
void HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef *hadc){
//elaborate ADCbuf[0...19]
}
...
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc){
//elaborate ADCbuf[20...39]
}
...
HAL_ADC_Start_DMA(&hadc1, (uint32_t *)ADCbuf, 40);

Thanks,
Luca

KnarfB
Super User
Jul 7, 2025 5:41 PM UTC

exactly. 

Spaghetto
SpaghettoAuthor
Associate III
Jul 14, 2025 10:45 AM UTC

Just a quick follow-up on the design above, implementing the two-step (4x)10 sample acquisition scheme the code is running smoothly without any overruns. Thanks for the hint.

Initializations:

Spoiler
__attribute__((section(".dma_buffer"))) uint16_t 	ADCbuf[40]={0};		//ADC to DMA buffer (4ch * #samples)
...
 //ADC Start
 if(HAL_ADC_Start_DMA(&hadc1, (uint32_t *)ADCbuf, 40) != HAL_OK){
		usb_print("ADC start KO!!!\r\n");
	 	HAL_GPIO_WritePin(LED_GPIO_Port, LED_Pin, RESET);
 Error_Handler();
 }

Callbacks:

Spoiler
void HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef *hadc){ //todo: ADC Half callback
	for(uint8_t i=0;i<4*GROUP/2;i+=4){

		//Add val^2 to sum (RMS)
		SumR[0] += ((uint32_t)ADCbuf[0+i]-Xoff)*(ADCbuf[0+i]-Xoff);
		SumR[1] += ((uint32_t)ADCbuf[1+i]-Xoff)*(ADCbuf[1+i]-Xoff);
		SumR[2] += ((uint32_t)ADCbuf[2+i]-Xoff)*(ADCbuf[2+i]-Xoff);
		SumR[3] += ((uint32_t)ADCbuf[3+i]-Xoff)*(ADCbuf[3+i]-Xoff);
	}
}

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc){ //todo: ADC Cplt callback
		for(uint8_t i=4*GROUP/2;i<4*GROUP;i+=4){
			//Add val^2 to sum (RMS)
			SumR[0] += ((uint32_t)ADCbuf[0+i]-Xoff)*(ADCbuf[0+i]-Xoff);
			SumR[1] += ((uint32_t)ADCbuf[1+i]-Xoff)*(ADCbuf[1+i]-Xoff);
			SumR[2] += ((uint32_t)ADCbuf[2+i]-Xoff)*(ADCbuf[2+i]-Xoff);
			SumR[3] += ((uint32_t)ADCbuf[3+i]-Xoff)*(ADCbuf[3+i]-Xoff);
		}

		if(Index>=Astop){ //Buffer full (end of frame acquisition)

			#ifdef OVERRUN_LOCK
			if(ADCcmplt){
				HAL_TIM_PWM_Stop(&htim1, TIM_CHANNEL_1);
				Overrun=1;
			}
			#endif

			//Transfer SumR and Reset
			SumRO[0]=SumR[0];
			SumRO[1]=SumR[1];
			SumRO[2]=SumR[2];
			SumRO[3]=SumR[3];
			SumR[0] = 0;
			SumR[1] = 0;
			SumR[2] = 0;
			SumR[3] = 0;

			Index = Astart; //Reset Index
			ADCcmplt=1;
		}
		else Index+=8*GROUP; //Index is calculated on SDRAM memory
}

Main:

Spoiler
 while (1){ //todo: Main Loop

	 if(ADCcmplt){ // Print data on Buffer full (was: TIM14 interrupt (10Hz) )

			sprintf(text,"A:%.6f,B:%.6f,C:%.6f,D:%.6f\r", //SumR and SumA are already computed, need just to sqrt(sum/N) and convert to volts
					(q*sqrt	(SumRO[0]/Xcnt))/k[j[0]],	//CH1 RMS
					(q*sqrt	(SumRO[1]/Xcnt))/k[j[1]],	//CH2 RMS
					(q*sqrt	(SumRO[2]/Xcnt))/k[j[2]],	//CH3 RMS
					(q*sqrt	(SumRO[3]/Xcnt))/k[j[3]]	//CH4 RMS
					);

			usb_print(text);


			HAL_GPIO_TogglePin(LED_GPIO_Port, LED_Pin);
			ADCcmplt=0; //Retrigger system output
	 }
	 HAL_Delay(1);
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }

Even if code is ok, and data has been validated with bench tests comparing data with lab instrumentation I'm still confused by the data read during debugging in STM32CubeIDE. Let me expand:
1- I've ADCdata[40] buffer initialized to {0},
2- Breaking code execution on the very first execution of HAL_ADC_ConvHalfCpltCallback(), I get all the 40 samples, not only the first 20 ones!

Spaghetto_1-1752489210512.png

3. Breaking code execution on the very first execution of HAL_ADC_ConvHalfCpltCallback(), I get all the 40 samples overwritten, not only the latter 20s!

Spaghetto_2-1752489225795.png

And so on...

I was expecting only a partial update (Half: 0-19 and Cmplt 20-39) but this is not happening. Am I misinterpreting how the callbacks are called?

Thanks,
Luca

KnarfB
Super User
Jul 16, 2025 5:06 AM UTC

Do you freeze the timer while debugging?

DBGMCU->APB2FZ |= DBGMCU_APB2_FZ_DBG_TIM1_STOP;

In addition, you may invalidate the data you have just processed in the callback to prove that there is fresh data in the buffer at the next callback.

For further validation, you could apply some well known waveform (sine, sawe tooth), dump and analyze the dumped DMA buffer data.

hth

KnarfB