Skip to main content
Associate III
November 23, 2023
Solved

ADC signal noise

  • November 23, 2023
  • 2 replies
  • 1435 views

Hi, I'm using stm32f429 disc1 adc1 PA4 and GND to get the ADC signal, the voltage of the signal is 300 mV. The signal that I'm getting after conversion has some noise, But the same signal when seen through an oscilloscope has no noise. The noise or distortions are getting generated once I connect to the pins of the powered-on board.

This topic has been closed for replies.
Best answer by KDJEM.1

Hello @harry123 ,

It is mentioned in the errata sheet ES0206 that some internal noise may impacting the ADC accuracy and workaround option is suggested.

For more detailed workaround, I advise you to refer to the application note "How to improve ADC accuracy when using STM32F2xx and STM32F4xx microcontrollers"  AN4073.

I hope this help you.

Thank you.

Kaouthar

2 replies

TDK
November 23, 2023

General tips to improve accuracy are here:

https://www.st.com/resource/en/application_note/an2834-how-to-optimize-the-adc-accuracy-in-the-stm32-mcus-stmicroelectronics.pdf

 

Should generally expect at least a few counts of noise for 12-bit measurements. More for high-impedance signals.

"If you feel a post has answered your question, please click ""Accept as Solution""."
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
November 23, 2023

Hello @harry123 ,

It is mentioned in the errata sheet ES0206 that some internal noise may impacting the ADC accuracy and workaround option is suggested.

For more detailed workaround, I advise you to refer to the application note "How to improve ADC accuracy when using STM32F2xx and STM32F4xx microcontrollers"  AN4073.

I hope this help you.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.