Skip to main content
ezrab
Associate III
November 25, 2010
Question

ADC Scan MODe

  • November 25, 2010
  • 6 replies
  • 1126 views
Posted on November 25, 2010 at 15:38

hi.

i have aquestion.

if i use the scan mode to measure sevrel channels at the end of the list of channel to measure how can i collect all the data from all the channels?

or do i have collect the data after every measre?

thanks for your help.
    This topic has been closed for replies.

    6 replies

    STM32 hobbyist
    Associate II
    November 25, 2010
    Posted on November 25, 2010 at 17:36

    You can refer to AN3116: ''STM32's ADC modes and their applications''. It shows you how to use the ADC its different modes with correspendant example.

    ezrab
    ezrabAuthor
    Associate III
    November 28, 2010
    Posted on November 28, 2010 at 07:01

    hi.

    thanks for the replay the document was good but only explainas the general option not how.

    my question still remains how can i collect all the sampelling data after ''Multichannel (scan), single conversion mode''

    where will it be stored?

    is there an exampe to ''Multichannel (scan), single conversion mode''?

    thanks

    ezrab
    ezrabAuthor
    Associate III
    November 28, 2010
    Posted on November 28, 2010 at 07:19

    as far as i can understand this can be done with DMA to transfer the result of the conversion to the RAM but the DMA has only 7 channels what if i need more like 9 conversion?

    is there away to do it?

    thanks.

    Tesla DeLorean
    Guru
    November 28, 2010
    Posted on November 28, 2010 at 16:07

    as far as i can understand this can be done with DMA to transfer the result of the conversion to the RAM but the DMA has only 7 channels what if i need more like 9 conversion?

     

     

    is there away to do it?

     

     

    And of those 7 DMA channels, exactly how many are connected to the ADC(s)? There is a diagram and table in the TRM that would be worth reviewing.

    I haven't dug into this, but surely it would use a SINGLE DMA channel, and interleave/sequence the readings? And use a large linear, or circular buffer.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    ezrab
    ezrabAuthor
    Associate III
    November 29, 2010
    Posted on November 29, 2010 at 07:54

    ''use a SINGLE DMA channel, and interleave/sequence the readings? And use a large linear, or circular buffer.''

     

     

    sounds great but where can i find how to do that?

    thanks.
    ezrab
    ezrabAuthor
    Associate III
    November 29, 2010
    Posted on November 29, 2010 at 08:02

    never mind i found it here AN3116

    at scan ScanContinuous example.

    thanks.