Skip to main content
RJOY.1
Associate II
April 16, 2021
Question

ADC Reading Error in STM32H743IIT6,100mV variation in each ADC reading.

In one of my project I am using STM32H743IIT6. I have to read multiple ADC sensors. We are following single conversion method with 10 bit resolution. But the issue is, when we read the ADC value, there is an increase of 100 mV in each ADC reading than actual value read from hardware. Any one can help me to avoid the issue?

Thanks in advance

Rose

This topic has been closed for replies.