ADC Reading Consistency
I am feeding 1.75V into an ADC input on a STM32F407 and see the voltage source is clean and consistent on a scope. I continuously read the value every 20ms. I see the ADC value change between 2108 to 2130. How consistent should the value be? I'm guessing it's not likely I will see the exact same value each time the ADC is read, but am wondering if the range I'm seeing is what should be expected as 'stable' reading. I'm using a separate 3.3V source for the analog. If I use a 4 layer board and separate analog ground, what is the consistently I should expect to see in consecutive ADC readings? I'm turned up all of the ADC peripheral settings to see if consistency would improve but it stays in the same range.
Thanks,