Skip to main content
ikrosoft
Associate II
Mar 26, 2021 2:17 PM UTC
Solved

ADC output suddenly becomes constant

Hello,

I'm using the ADC on a STM32G431 to read 5 voltages at 20kHz. Everything works well, but suddenly the 5 channels "get stuck" or freeze, i.e. the value they measure becomes constant even though the voltages on the input pins still fluctuate. Sometimes the measured values resume to being correct again by themselves after a little while (like after 200 samples for instance), other times the values remain constant until I manually cycle the MCU power.

Some more details about the code architecture:

  • I use 5 channels of the ADC2 in single-ended mode
  • The sequence of 5 regular conversions (Single conversion mode) is triggered by TIM2's TRGO (update event at 20kHz)
  • Data is stored in an array by DMA in circular mode. In the DMA ISR I have code to copy and log this data (at each DMA transfer complete interrupt).

Some info about my debugging so far:

  • I've enabled ADC overrun interrupt and checked that it never gets fired
  • Same goes for the DMA transfer error
  • When logging the data I also log a timestamp (the value of a free running timer) to be certain that it's not my logging that gets stuck or that I'm seeing a scheduling problem. No issue there, the DMA ISR (and thus the logging) always gets called at 20kHz.
  • Although the ADC measures are unrelated, this same PCB is also powering a motor. And it looks like it's when the motor has to performs an abrupt speed step that the ADC values get stuck. But I've looked at VDDA (= Vref+) with an oscilloscope, and there's no particular glitch to be seen when the values get stuck.

NB: this is surprisingly similar to this question by @FChen.3​ , but since no answer was given there I thought sharing my case still is useful.

This topic has been closed for replies.
MM..1
MM..1Best answer
Super User
Mar 2, 2023 6:24 AM UTC
First learn teory... PWM is modulation type and need demodulate before measure.
Schematics is PWM out – R – C to gnd R and C need calculate based on freq and max pin current ...
Demodulated voltage can you measure on C.

12 replies

MM..1
Super User
Mar 26, 2021 3:50 PM UTC

Try configure MCU clock without PLL (HSI or HSE)

ikrosoft
ikrosoftAuthor
Associate II
Mar 31, 2021 8:22 AM UTC

Thanks for you answer.

Sadly I can't do without the PLL (the MCU needs to be running at almost max speed), but still I've managed to reduce the PLL_N multiplication factor from 84 to 21. It looks like it's not helping though, the ADC still freezes.

Why do you point at the PLL? Is there some known bugs or undocumented limitations?

As suggested in the aforementioned thread, I've tried to restart the ADC + DMA when ADC freeze is detected. This indeed allows resuming ADC operation back to normal, but it's not really a solution.

Any other ideas of what could cause the observed ADC freezes?

Igor Cesko
ST Employee
Apr 13, 2021 2:09 PM UTC

Hi ikrosoft (Community Member),

Please check if the VREF+ / VSSA decoupling is perfect. Capacitors (1uF + 100nF) must be located very very close to the VREF+/VSSA pins. Please read recommendations for ADC in application note AN5346.

Regards

Igor

ikrosoft
ikrosoftAuthor
Associate II
Apr 27, 2021 8:19 AM UTC

Hi Igor,

Thanks for your input. VDDA/VSSA pins are indeed well decoupled using 1uF+100nF ceramic caps placed ~1mm from the pins, but the caps are on the other side. I'll try and move them to the same side just in case.

Best,

ikrosoft

Igor Cesko
ST Employee
Apr 27, 2021 8:36 AM UTC

Hi ikrosoft (Community Member),

What is the ADC clock? What is the "constant" ADC value (output word from ADC)? Which device revision are you using? Try to replace DMA with interrupt or polling method - to identify if the problem is in the DMA or not.

Regards

Igor

jtron.1
Associate II
Feb 28, 2023 12:08 PM UTC

Hi All.

I am trying to use STM32F103 devices ADC channel number 0 and 1.

I checked the voltage over the pin IN0 and IN1 is 0.8V to 0.99V without giving any input to the pin due to this I am getting wrong value.

Could you please tell me the cause for this??

Thanks

Igor Cesko
ST Employee
Feb 28, 2023 1:14 PM UTC

Hi jtron.1,

If ADC input pin is floating then the input voltage is undefined and if you are measuring this floating pin the voltage is some residual voltage on sampling capacitor.

Why are you not providing some voltage on IN0 and IN1 an measuring it?

Regards

Igor

jtron.1
Associate II
Feb 28, 2023 4:51 PM UTC

Thanks for the reply Igor.

Will residual voltage affect the accuracy?

When I try to pull this voltage down then I got 0000 reading on my display.

Can I use external pull down resistor.??

My concern is this the floating pin voltage is about 900mV to 1V so if I apply voltage less than 900mV will it work?

Because I want to measure voltage less than 600mV.

I did not provide yet as I was stuck in floating voltages I am getting on IN0 and IN1.

Thanks...

Igor Cesko
ST Employee
Mar 1, 2023 3:46 PM UTC

Hi jtron.1,

The voltage on floating ADC input pin is very weak - so external signal easily force own voltage on pin. The source signal impedance must follow the datasheet requirements: impedance less than 50 kOhm.

Regarding the voltage on IN0 and IN1 : what is the ADC result (data from ADC) for those channels? Are they zero or another values? And is this value fixed also if input volatge is changing?

Regards

Igor

jtron.1
Associate II
Mar 2, 2023 4:28 AM UTC

Hi Igor,

Actually I am trying to measure the voltage of PWM signal at 1kHz with 50% duty cycle. Now the signal I am measuring having amplitude 3.1V checked on CRO and the ADC considering this and showing the results as per this for instance Vref is 3.3V ADC is 12-Bit. (4095/3.3)xADC_IN0=3846 which is I am getting with slightly jumping that is not a problem for now. But, when I check the voltage with multimeter it is showing 1.6V now I am confusing what's going on.?

I want to just measure the PWM signal with right way.

Also tried one thing I used 1uF,25V electrolytic capacitor just after the PWM signal and 10K resistance in series with ADC pin by doing this it is showing right value as per the multimeter. I am not sure that it is right way to measure the PWM signal or not.

Am I doing right or wrong here pl let me know??

What sort of thing I should be taken care of while measuring PWM signal.?

MM..1
MM..1Best answer
Super User
Mar 2, 2023 6:24 AM UTC
First learn teory... PWM is modulation type and need demodulate before measure.
Schematics is PWM out – R – C to gnd R and C need calculate based on freq and max pin current ...
Demodulated voltage can you measure on C.
jtron.1
Associate II
Mar 2, 2023 6:48 AM UTC

Ok thanks for the reply.