Skip to main content
Associate III
May 30, 2024
Question

ADC on STM32G030K8 inconsistent voltage measurements

Hi, I am using battery voltage charging as a part of my project. For some reasons my voltage reading in the prototype is 1.18 V and the ADC reading in my debugger is 1.25 V. This totally different for different module. Physically all modules are measuring 1.18 V across the resistors but ADC reading in debugger changes to 1.22 ,1.26,1.28.

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
May 30, 2024

What do your schematics around the STM32G0 look like?

Which ADC parameters have you set?

What does your measuring routine look like?

Without such basic information, we will not be able to help you.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.