Skip to main content
Pzhu.1
Associate II
August 28, 2021
Solved

ADC of STM32F401RC sometimes do not work

Hi,

I configure the ADC as the following code; but sometimes(not everytime) the code will run to Line 70 : "Beer_Out_Dis(1);" ,and ADC will not work.

Did I do something wrong? Thanks verymuch.

/* ADC1 init function */
static void MX_ADC1_Init(void)
{
 
 ADC_ChannelConfTypeDef sConfig;
 
 /**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) 
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.ScanConvMode = ENABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.NbrOfConversion = 7;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 HAL_ADC_Init(&hadc1);
 
 /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. 
 */
 sConfig.Channel = ADC_CHANNEL_0; //USB -> PA0 Voltage
 sConfig.Rank = 1;
 sConfig.SamplingTime = ADC_SAMPLETIME_28CYCLES;
 HAL_ADC_ConfigChannel(&hadc1, &sConfig); 
 
 /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. 
 */
 sConfig.Channel = ADC_CHANNEL_1; //USB -> PA1 Current
 sConfig.Rank = 2;
 HAL_ADC_ConfigChannel(&hadc1, &sConfig); 
 
 /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. 
 */
 sConfig.Channel = ADC_CHANNEL_4; // J2 -> PA4
 sConfig.Rank = 3;
 HAL_ADC_ConfigChannel(&hadc1, &sConfig); 
 
 /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. 
 */
 sConfig.Channel = ADC_CHANNEL_5; // J10 -> PA5
 sConfig.Rank = 4;
 HAL_ADC_ConfigChannel(&hadc1, &sConfig);
 
 /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. 
 */
 sConfig.Channel = ADC_CHANNEL_6; // J4 -> PA6
 sConfig.Rank = 5;
 HAL_ADC_ConfigChannel(&hadc1, &sConfig); 
 
 /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. 
 */
 sConfig.Channel = ADC_CHANNEL_7; // J13 -> PA7
 sConfig.Rank = 6;
 HAL_ADC_ConfigChannel(&hadc1, &sConfig);
 
 /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. 
 */
 sConfig.Channel = ADC_CHANNEL_9; //POWER ->PB1
 sConfig.Rank = 7;
 HAL_ADC_ConfigChannel(&hadc1, &sConfig);
 
 HAL_ADC_Start_DMA(&hadc1, (uint32_t*)&Ad_Data[0], 7);
 
 if ( HAL_ADC_Start(&hadc1)!=HAL_OK)
 {
 Beer_Out_Dis(1);
 }
 
}

This topic has been closed for replies.
TDK
TDKBest answer
August 28, 2021

Don't call both HAL_ADC_Start_DMA and HAL_ADC_Start. If it's busy with the first call, the second one will fail. If you want to use DMA, use HAL_ADC_Start_DMA. If you want to use polling, use HAL_ADC_Start.

https://github.com/STMicroelectronics/STM32CubeF4/blob/2f3b26f16559f7af495727a98253067a31182cfc/Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_adc.c#L87

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
August 28, 2021

Don't call both HAL_ADC_Start_DMA and HAL_ADC_Start. If it's busy with the first call, the second one will fail. If you want to use DMA, use HAL_ADC_Start_DMA. If you want to use polling, use HAL_ADC_Start.

https://github.com/STMicroelectronics/STM32CubeF4/blob/2f3b26f16559f7af495727a98253067a31182cfc/Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_adc.c#L87

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pzhu.1
Pzhu.1Author
Associate II
August 28, 2021

Thanks very much! I understand and I will modify the code.