ADC noise issue (pin PA0) STM32F746
- September 13, 2021
- 4 replies
- 1281 views
ADC noise issue (pin PA0) STM32F746 microcontroller
Please explain the presence of increased noise at the PA0 pin of the STM32F746ZGT6 microcontroller in the ADC mode.
ADC parameters:
• Clock frequency - 13.5 MHz (with a prescaler 4)
• Sampling frequency (period) 100 ms
• Sampling period 56 cycles
Below are oscillograms taken from the NUCLEO-F746ZG development board.
ES0290 Rev 7 clause 2.2.2 - did not help
The same noises are observed on the prototype of the assembled device - everything is exactly like on the NUCLEO-F746ZG.
Below is a part of the analog input of the product prototype on STM32F746ZGT6 - pin PA0.
There is no ripple in the power supply of the operational amplifier (OP484), the D10 input is not connected anywhere.
Plans to use all analog inputs.
Recommend a solution.