Skip to main content
KPerg.1
Associate II
January 11, 2023
Question

ADC Input protection

I will be using 16 channels of STM32 ADC and I would like to protect them against overvoltage and ESD (those will be used as device inputs and unwanted situations can happen), my initial thought was to use a Zenner diode array and current limiting resistor on each input. I am into the digital world and I'm not 100% sure if it will work and if it won't distort the input signal. Maybe you know a better solution for such a problem?

Thanks in advance for any help!

This topic has been closed for replies.

2 replies

S.Ma
Principal
January 12, 2023

That depends on the analog hw, impedence, etc... not one size fits all answer out there....

Use an follower opamp with low offset if you can afford it.

guillaumefaye
Associate II
May 27, 2024

I am in a similar situation, I use the internal reference 2.048v as a reference for the ADCs, for the protection of the ADC inputs should I use a zener of 3.3v (VDDA?) or 2v (vref)? THANKS.