ADC fluctuations problem
Hi,
I am having a problem with ADC read. The values I get from conversion are 100% random. They get from 0 to max range without any pattern. Example codes from MXCube work fine and the value is stable. My own code generated in cube is not fixing the issue. I tried to compare the example and my own code, but didnt find any difference besides CPUcache beeing enabled in example (that I ignored). Every other function in ADC works for me. Can anyone please tell me what am I doing wrong? Thanks in advance!
I am using KeiluVision 5.0 with STM32F767ZI on nucleo board. Here is my code
.
int main()
{
ADC_init();
ADC_port_init();
}
.
void ADC_port_init(void)
{ /////////// AHB for GPIOA RCC -> AHB1ENR |= RCC_AHB1ENR_GPIOAEN; . /////////// Pin A1 analog GPIOA -> MODER |= GPIO_MODER_MODER1_0 | GPIO_MODER_MODER1_1; . /////////// Pin A1 very high speed GPIOA -> OSPEEDR |= GPIO_OSPEEDER_OSPEEDR1_0 | GPIO_OSPEEDER_OSPEEDR1_1;}.
void ADC_init (void)
{ /////////// Conwerter ON ADC1 -> CR2 |= ADC_CR2_ADON; . /////////// APB for ADC init RCC->APB2ENR |= RCC_APB2ENR_ADC1EN; . /////////// Interrupt when EOC ADC1 -> CR1 |= ADC_CR1_EOCIE; . /////////// 12 bit resolution (11) ADC1 -> CR1 &= ~ADC_CR1_RES_0 & ~ADC_CR1_RES_0; . /////////// Single conversion ADC1 -> CR2 &= ~ADC_CR2_CONT; . /////////// EOC after regular group ADC1 ->CR2 &= ~ADC_CR2_EOCS; . /////////// Sample time 480 cycles (010) ADC1 ->SMPR2 |= ADC_SMPR2_SMP1_0 | ADC_SMPR2_SMP1_1 | ADC_SMPR2_SMP1_2; . /////////// 1 measurement in regular group (0000) ADC1 -> SQR1 &= ~ADC_SQR1_L_0 & ~ADC_SQR1_L_1 & ~ADC_SQR1_L_2 & ~ADC_SQR1_L_3;. /////////// First measurement on PA1 (0001) ADC1 -> SQR3 &= ~ADC_SQR3_SQ1_0 | ADC_SQR3_SQ1_1 & ~ADC_SQR3_SQ1_2 & ~ADC_SQR3_SQ1_3; . /////////// Start regular conversion ADC1 -> CR2 |= ADC_CR2_SWSTART;}#problem #adc #fluctuations #stm32f767zi