Skip to main content
gilles2399
Associate II
March 13, 2012
Question

ADC DMA problem

  • March 13, 2012
  • 2 replies
  • 635 views
Posted on March 13, 2012 at 11:43

ADC DMA problem

    This topic has been closed for replies.

    2 replies

    raptorhal2
    Lead
    March 13, 2012
    Posted on March 13, 2012 at 18:04

    At the moment, I am assuming that clocks and GPIOs are correctly initialized.

    I need a better description of the relationship between sampling trigger and square wave frequency. Is the sampling trigger frequency 1 MHz ? What is the square wave frequency ?  How are you sorting out the triple conversion results to reconstruct the square wave at the trigger frequency ?

    A signal 1 V pp suggests the signal is sometimes negative. Do you really mean that the signal goes from 0.5 mV to 1 V ?

    Cheers, Hal

    gilles2399
    Associate II
    March 19, 2012
    Posted on March 19, 2012 at 13:36

    Hello,

    Excuse me for the late reply

    I managed to fix the problem which is due to a little error on the clock configuration.

    Thanks for your reply.