Question
ADC+DMA fills all the buffer when calling to HAL_ADC_ConvHalfCpltCallback()
In a stm32f303rb76, I commanded to operate ADC+DMA by setting of the
ADC DMA with circular mode
The ADC I activated continuous conversion mode
and DMA continuous request
Also the analog input signal (no scan mode)
In the initialization made following command:
HAL_ADC_Start_DMA(&hadc1, (uint32_t*)adc1_buf, 2*ADC_BUF_LEN);
Then in the debug mode I realized that always calls:
HAL_ADC_ConvHalfCpltCallback()
filling all the buffer (not a half)
But never calls to HAL_ADC_ConvCpltCallback()
it is a problem of the debugger?
How can be solved?