ADC configuration with PC0 and PA0
I recognize that this is probably a dumb question but I'm really struggling with it. I've successfully configured ADCs for reads when using PA0 and PA1:
void
ADC_Setup
() {GPIO_InitTypeDef GPIO_InitStructure;
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
// enable clocks for GPIO and ADC
RCC_AHB1PeriphClockCmd
(RCC_AHB1Periph_GPIOA, ENABLE);RCC_APB2PeriphClockCmd
(RCC_APB2Periph_ADC1, ENABLE);// configure PA0, PA1 as alternate function inputs
GPIO_StructInit
(&GPIO_InitStructure);GPIO_InitStructure.
GPIO_Speed
= GPIO_Speed_2MHz;GPIO_InitStructure.
GPIO_Mode
= GPIO_Mode_AIN;GPIO_InitStructure.
GPIO_PuPd
= GPIO_PuPd_NOPULL;GPIO_InitStructure.
GPIO_Pin
= GPIO_Pin_0 | GPIO_Pin_1;GPIO_Init
(GPIOA, &GPIO_InitStructure);// ADC1 configuration
ADC_CommonStructInit
(&ADC_CommonInitStructure);ADC_CommonInitStructure.
ADC_Mode
= ADC_Mode_Independent;ADC_CommonInitStructure.
ADC_Prescaler
= ADC_Prescaler_Div2;ADC_CommonInitStructure.
ADC_DMAAccessMode
= ADC_DMAAccessMode_Disabled;ADC_CommonInitStructure.
ADC_TwoSamplingDelay
= ADC_TwoSamplingDelay_5Cycles;ADC_CommonInit
(&ADC_CommonInitStructure);ADC_StructInit
(&ADC_InitStructure);ADC_InitStructure.
ADC_Resolution
= ADC_Resolution_12b;ADC_InitStructure.
ADC_ScanConvMode
= DISABLE;ADC_InitStructure.
ADC_ContinuousConvMode
= DISABLE;ADC_InitStructure.
ADC_ExternalTrigConvEdge
= ADC_ExternalTrigConvEdge_None;ADC_InitStructure.
ADC_DataAlign
= ADC_DataAlign_Right;ADC_InitStructure.
ADC_NbrOfConversion
=1
;ADC_Init
(ADC1, &ADC_InitStructure);ADC_Cmd
(ADC1, ENABLE);}
uint16_t
ADC_GetChannel
(uint8_t
channel) {ADC_RegularChannelConfig
(ADC1, channel,1
, ADC_SampleTime_84Cycles);// Start the conversion
ADC_SoftwareStartConv
(ADC1);// Wait until conversion completion
while
(ADC_GetFlagStatus
(ADC1, ADC_FLAG_EOC) == RESET);// Get the conversion value
return
ADC_GetConversionValue
(ADC1);}
♯
define
CUTOFF_FREQUENCY
10
// Hz
// low-pass filter works using precomputed alpha = 0.5
uint16_t
filterVoltageFast
(uint16_t
oldVal,uint16_t
newSample) {return
oldVal + ((newSample - oldVal) >>1
);}
void
ADC_Poll
(volatile
ADC_Value *adc) {adc->brake[
1
] =ADC_GetChannel
(0
);adc->throttle[
1
] =ADC_GetChannel
(1
);adc->brake[
1
] =filterVoltageFast
(adc->brake[1
],ADC_GetChannel
(0
));adc->brake[
0
] = adc->brake[1
];adc->throttle[
1
] =filterVoltageFast
(adc->throttle[1
],ADC_GetChannel
(1
));adc->throttle[
0
] = adc->throttle[1
];}
Which works. Now I'm trying to convert this to work with PA0 and PC0 for the same functionality, just with different pins, and I can't figure out where I'm going wrong. With PA0 and PA1 code
does a bit of additional checks with the low pass filter but I've stripped this down to as little as I think it should be able to get by with, and no dice. Currently it reads kind of random values no matter what voltage I apply to the pin.
void dev_adc_setup() {
GPIO_InitTypeDef GPIO_InitStructure_Throttle; GPIO_InitTypeDef GPIO_InitStructure_Brake; ADC_InitTypeDef ADC_InitStructure; ADC_CommonInitTypeDef ADC_CommonInitStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC3, ENABLE); ADC_DeInit(); // THROTTLE GPIO SETUP // RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); GPIO_StructInit(&GPIO_InitStructure_Throttle); GPIO_InitStructure_Throttle.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure_Throttle.GPIO_Mode = GPIO_Mode_AIN; GPIO_InitStructure_Throttle.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure_Throttle.GPIO_Pin = GPIO_Pin_0; GPIO_Init(GPIOA, &GPIO_InitStructure_Throttle); // BRAKE GPIO SETUP // RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); GPIO_StructInit(&GPIO_InitStructure_Brake); GPIO_InitStructure_Brake.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure_Brake.GPIO_Mode = GPIO_Mode_AIN; GPIO_InitStructure_Brake.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure_Brake.GPIO_Pin = GPIO_Pin_0; GPIO_Init(GPIOC, &GPIO_InitStructure_Throttle); // ADC1 configuration ADC_CommonStructInit(&ADC_CommonInitStructure); ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles; ADC_CommonInit(&ADC_CommonInitStructure); ADC_StructInit(&ADC_InitStructure); ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; ADC_Init(ADC3, &ADC_InitStructure); ADC_Cmd(ADC3, ENABLE);}uint16_t dev_readADC(uint8_t channel){ ADC_RegularChannelConfig(ADC1, channel, 1, ADC_SampleTime_84Cycles); // start the conversion ADC_SoftwareStartConv(ADC1); // wait until conversion completion while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET); // get the conversion value return ADC_GetConversionValue(ADC1); }#adc-init #adc-reads #adc #stm32f4-adc #adc-config #adc-stm32 #adc-help