Question
ADC Clock config
Posted on October 24, 2013 at 16:13
Hi there,
Lately I'm experimenting with the STM32FXXX. Now I came across a problem when I want to configurate the ADC clock. I want to use the maximum frequency that is possible for the ADC. The manual says that the maximum clock frequency for the ADC is 14MHz.I also want to use the maximum speed for my systemclock which is 72MHz. When I want to scale the ADC clock to 14MHz I can only devide by 2,4,6,8 of 72MHz. This results into 18MHz or 12MHz for the ADC clock.Will the ADC clock works at 14MHz if it is set at 18MHz? Or will I get some trouble afterwards?void RCC_Configuration(void) { RCC_HSICmd(ENABLE);FLASH_SetLatency(FLASH_Latency_2);
RCC_PLLConfig(RCC_PLLSource_HSI_Div1, RCC_PLLMul_9);
RCC_PLLCmd(ENABLE); while (RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET); RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);RCC_HCLKConfig(RCC_SYSCLK_Div1);
RCC_PCLK1Config(RCC_HCLK_Div2); RCC_PCLK2Config(RCC_HCLK_Div1);}