Skip to main content
Visitor II
February 16, 2026
Question

ADC and DAC issue-Hardware

I’m using an STM32F439VIT6 on a custom board. PA5 is used as the DAC output, and PA0/PA1 as the ADC inputs. On 1 out of 5 boards, the ADC and DAC functions stopped working, but the same pins still work correctly as GPIO.

Setup (failing board)

PA5: DAC → op-amp → 0–10 V output

PA0, PA1: ADC inputs from INA190A1 for 4–20 mA sensors

VDDA/VREF+ = 3.3 V (measured OK)

Same firmware as working boards

Pins configured in analog mode

Issue

DAC produces no valid analog output, always zero

ADC readings are invalid or stuck

GPIO input/output on the same pins works

Question

Can the STM32F4 analog (ADC/DAC) circuitry be damaged while the GPIO still works on the same pins?

How can I confirm if the ADC/DAC core is damaged (e.g., internal channels/tests)

3 replies

Andrew Neil
Super User
February 16, 2026

Welcome to the forum.

Please see: How to write your question to maximize your chances to find a solution

In particular, as it's a custom board, please post the schematic.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
February 16, 2026

> On 1 out of 5 boards, the ADC and DAC functions stopped working, but the same pins still work correctly as GPIO.

What did you do when it stopped working? It sounds like the board has been damaged.

 

> Can the STM32F4 analog (ADC/DAC) circuitry be damaged while the GPIO still works on the same pins?

Sure. If the chip is damaged, the behavior is generally undefined. It is not uncommon for one function to fail but for others to work if the board has been subjected to damage.

> How can I confirm if the ADC/DAC core is damaged (e.g., internal channels/tests)

There's no 100% test here. But using the same code as on other boards to verify internal temperature and VREFINT channels would be a good start. If those are not working correctly, and the hardware is otherwise correct (e.g. no solder bridges or cold/missing connections) then the board is damaged.

"If you feel a post has answered your question, please click ""Accept as Solution""."