Skip to main content
MMurr.2
Associate II
February 16, 2023
Question

ADC always returns 0

I'm trying to read 2 ADC channels (ch 0-1) on an STM32G030C8T6 but the only result I can get from the ADC is a 0.

I've confirmed the voltages I'm trying to read are at ~1.6V and that the VREF+ pin is at ~2.7V using a multimeter so I dont believe its a hardware issue.

Looking at the SFRs in debug mode just before starting a conversion, all configuration registers seem normal and exactly as they were set in the device configuration tool, the GPIO MODER registers are set to analog, and the ADC clock is enabled in RCC. There were just two things that stood out to me which may or may not mean anything.

  1. When trying to do this using interrupts, the SFRs tab of the debugger would say that EOC in the ADC_ISR register is set, but if I assigned it to a variable or made a comparison to it in code, it would be unset. I.E the expression ((ADC1->ISR & ADC_ISR_EOC) == ADC_ISR_EOC) would evaluate to false even if the debugger said the EOC bit was set.
  2. The OVR and EOS flags in the ADC_ISR register are always set after a conversion, even if it was just a single conversion so there shouldnt have been a EOC flag set to trigger the OVR flag. The attached image is the ISR register directly after the first conversion in the code provided.

I've tried using "Sequencer set to fully configurable" and "Sequencer not set to fully configurable" modes along with continuous, discontinuous, and scan conversion modes and both possible overrun behaviours.

Edit forgot to add: The hadc1 instance doesn't report any errors and no errors get returned from any function.

If anyone has any ideas on what this could be it would be greatly appreciated since at this point I'm lost on where to go from here.

/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
 
/* USER CODE BEGIN PV */
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_ADC1_Init(void);
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_ADC1_Init();
 /* USER CODE BEGIN 2 */
 
 HAL_ADCEx_Calibration_Start(&hadc1);
 uint16_t ADC_result;
 
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	 HAL_Delay(1000);
	 HAL_GPIO_TogglePin(LED_GPIO_Port, LED_Pin);
 
	 HAL_ADC_Start(&hadc1);
	 HAL_ADC_PollForConversion(&hadc1, 1000);
	 ADC_result = HAL_ADC_GetValue(&hadc1);
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Configure the main internal regulator output voltage
 */
 HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
 
 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1;
 RCC_OscInitStruct.PLL.PLLN = 8;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/**
 * @brief ADC1 Initialization Function
 * @param None
 * @retval None
 */
static void MX_ADC1_Init(void)
{
 
 /* USER CODE BEGIN ADC1_Init 0 */
 
 /* USER CODE END ADC1_Init 0 */
 
 ADC_ChannelConfTypeDef sConfig = {0};
 
 /* USER CODE BEGIN ADC1_Init 1 */
 
 /* USER CODE END ADC1_Init 1 */
 
 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_SEQ_FIXED;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.LowPowerAutoPowerOff = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.DMAContinuousRequests = DISABLE;
 hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
 hadc1.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_160CYCLES_5;
 hadc1.Init.OversamplingMode = DISABLE;
 hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_0;
 sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_1;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */
 
 /* USER CODE END ADC1_Init 2 */
 
}
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOA_CLK_ENABLE();
 
 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(LED_GPIO_Port, LED_Pin, GPIO_PIN_RESET);
 
 /*Configure GPIO pin : LED_Pin */
 GPIO_InitStruct.Pin = LED_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(LED_GPIO_Port, &GPIO_InitStruct);
 
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

0693W00000YAqalQAD.png

This topic has been closed for replies.

7 replies

Walid ZRELLI
Visitor II
February 16, 2023

Hello @MMurr.2​ ,

You must enable the ADC interrupt mode and configure the NVIC.

In addition, you must use this HAL_ADC_Start_IT() function to start the conversion of a regular group with interrupt. The interrupts enabled in this function according to the initialization parameters: EOC (end of conversion), EOS (end of sequence) and OVR overrun.

Otherwise, have a look at this video, it might help you.

BeST Regards,

Walid

MMurr.2
MMurr.2Author
Associate II
February 16, 2023

I have done this, I just provided the minimum reproducible code for asking this question. The ISR gets called when a conversion is done but the data register is still always 0.

waclawek.jan
Super User
February 17, 2023

Try a single channel. Try the internal VREFINT channel.

Read out and check/post ADC and relevant GPIO registers content.

Looking at ADC registers is intrusive - some bits are cleared by reading the data register.

JW

MMurr.2
MMurr.2Author
Associate II
February 17, 2023

So I just tried it again today to try this and it worked perfectly - no changes to code or configuration whatsoever.

I am incredibly confused on what could've caused this but its working so I guess its ok now. Maybe my board just felt temperamental that day.

Javier1
Principal
February 18, 2023

@MMurr.2​ , If its a custom assembled board i'd check for cold solder mcu pins

hit me up in https://www.linkedin.com/in/javiermuñoz/
S.Ma
Principal
February 18, 2023

Make sure: Flash the MCU and set an output when ADC is working, power down and up the board and check. This to avoid "need to do a hot reset to kick the ADC on" or "it works only when debugging"

bsfrn
Associate
June 26, 2024

Hi, did you find any solution?