Skip to main content
greg_t
Associate III
July 30, 2010
Question

ADC 1

  • July 30, 2010
  • 4 replies
  • 731 views
Posted on July 30, 2010 at 12:17

ADC 1

    This topic has been closed for replies.

    4 replies

    raptorhal2
    Lead
    May 17, 2011
    Posted on May 17, 2011 at 14:00

    Each ADC has one conversion data register, not one register per channel, so you need to use DMA for two or more channels.

    Cheers, Hal

    greg_t
    greg_tAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:00

    /* Enable ADC1 clock */

      RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);

    // RC5 - analog input - ADC

      GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;

      GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;

      GPIO_Init (GPIOC, &GPIO_InitStructure);

      

    ADC_InitTypeDef ADC_InitStructure;

      

      ADC_DeInit(ADC1);

      

    // ADC Structure Initialization

      ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;

      ADC_InitStructure.ADC_ScanConvMode = DISABLE;

      ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;

      ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None; 

      ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

      ADC_InitStructure.ADC_NbrOfChannel = 2;

      // Enable Temperature channel

      ADC_TempSensorVrefintCmd ( ENABLE );

      // Init ADC1

      ADC_Init ( ADC1, &ADC_InitStructure );

    ADC_RegularChannelConfig ( ADC1 , ADC_Channel_15 , 1 , ADC_SampleTime_41Cycles5 );

    ADC_RegularChannelConfig ( ADC1 , ADC_Channel_16 , 2 , ADC_SampleTime_239Cycles5 );

      // Enable the ADC

      ADC_Cmd ( ADC1, ENABLE );

      // ADC calibration

      // Enable ADC1 reset calibaration register

      ADC_ResetCalibration(ADC1);

      // Check the end of ADC1 reset calibration register

      while(ADC_GetResetCalibrationStatus(ADC1) == SET);

      // Start ADC1 calibaration

      ADC_StartCalibration(ADC1);

      // Check the end of ADC1 calibration

      while(ADC_GetCalibrationStatus(ADC1) == SET);

      

    /* Function for ADC1 read

    int32_t GetADC1Channel(void)

    {

      

      // Start the conversion

      ADC_SoftwareStartConvCmd(ADC1, ENABLE);

      // Wait until conversion completion

      while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);

      

      // Get the conversion value

      return (int32_t)((ADC_GetConversionValue(ADC1)*100)/4095);  // return percentage

    }

    raptorhal2
    Lead
    May 17, 2011
    Posted on May 17, 2011 at 14:00

    Post your code so we can see if everything is initialized properly.

    Cheers, Hal

    greg_t
    greg_tAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:00

    Thanks