Skip to main content
phani
Associate II
Jan 12, 2009 5:19 PM UTC
Question

Access external flash part using I2C/SPI Interface

Posted on January 12, 2009 at 18:19

Access external flash part using I2C/SPI Interface

    This topic has been closed for replies.

    1 reply

    phani
    phaniAuthor
    Associate II
    May 17, 2011 10:58 AM UTC
    Posted on May 17, 2011 at 12:58

    I need to connect an external NAND/NOR flash to STM32F101Vx.

    The option that I am considering is to use is the FSMC interface. In this way this part of the memory will be accesible using the ''uVision'' IDE and related flash loaders.

    I have to interface a LCD Module too, which requires the FSMC interface. Given this scneario do you think I can connect the external flash using I2C/SPI interface and still be able to access the flash part.

    I want this flash part to be addressable directly as part of the program memory space.

    Thanks in advance for your help