Skip to main content
Issamos
Super User
Nov 10, 2025 8:36 PM UTC
Solved

About the DS11532

Hello ST Community team,

On the DS11532: 

  • The title of the Figure 20 should be changed to avoid any confusion between figure 20 and figure 21.
  • Also, the note under figure1 is not really clear since the STM32F767 TFBGA216 for example is not compatible pin to pin with the STM32F469 TFBGA216. So, I think the note should be clearer. It can even point to the application note AN4660 for details.

Could you please have a look.

Best Regards.

II

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Nov 10, 2025 9:52 PM UTC

Hi @Issamos ,

There is no duplication for Figure 20 and 21 as: Figure 20. is for STM32F76xxx TFBGA216 and Figure 21. for STM32F769xx TFBGA216 with DSI.

I escalated your issue regarding the text below the figure1 to clarify this (internal ticket number: 221536).

Thank you for your contributions.

(PS: Internal ticket number 221536 is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

3 replies

ST Technical Moderator
Nov 10, 2025 8:41 PM UTC

Hello @Issamos ,

Thank you for having reported this.
I will check this and come-back to you soon with updates.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Imen.DBest answer
ST Technical Moderator
Nov 10, 2025 9:52 PM UTC

Hi @Issamos ,

There is no duplication for Figure 20 and 21 as: Figure 20. is for STM32F76xxx TFBGA216 and Figure 21. for STM32F769xx TFBGA216 with DSI.

I escalated your issue regarding the text below the figure1 to clarify this (internal ticket number: 221536).

Thank you for your contributions.

(PS: Internal ticket number 221536 is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Nov 14, 2025 1:14 PM UTC

Hi @Issamos ,
After deep check, we have concluded that the STM32F76x and STM32F4xx devices are indeed pin-to-pin compatible when not considering packages that include the DSI peripheral.

So, the following sentence in DS11532 under Figure 1 (page 19) :

"The STM32F76x LQFP144, LQFP176, LQFP208, TFBGA216, UFBGA176 packages are fully pin to pin compatible with STM32F4xx devices."

will be changed to:
“The STM32F76x and STM32F4xx devices are indeed pin-to-pin compatible when not considering packages that include the DSI peripheral.”

For further details, I recommend consulting AN4660, section 1.1.4 “TFBGA216 package,” which provides a through explanation of this compatibility.

Thank you for your contribution.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks