Skip to main content
v_tamakov
Associate
June 14, 2018
Question

About SWD signals

  • June 14, 2018
  • 2 replies
  • 1679 views
Posted on June 14, 2018 at 16:00

Hello, please tell me, what is the minimum number of signals required for the SWD interface: SWDIO, SWCLK? NRST is also required or possible without it?

    This topic has been closed for replies.

    2 replies

    Vitaliy Chernobay
    Senior
    June 14, 2018
    Posted on June 14, 2018 at 21:14

    NRST is desirable to have, but it works without it

    Tesla DeLorean
    Guru
    June 15, 2018
    Posted on June 15, 2018 at 18:05

    SWO (PB3) is also generally desirable, although not helpful on CM0(+) device, and currently broken on H7.

    Some debuggers need VTarget to power buffers in the pod, and obviously you need a common ground.

    If you don't have room for headers or test points, consider edge castellations, or break-off portions of the PCB

    Consider your needs for manufacturing test and product development when scoping what is in fact 'minimal'

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Geoffrey1
    Associate III
    June 15, 2018
    Posted on June 15, 2018 at 03:05

    You definitely want nRST.   It is possible to configure the stm32 components so that the debugger interface is disabled or the pins are reconfigured (e.g. st32l4 parts in standby or shutdown).  In this situation, the only way to connect the debugger is to reset the part.  It may not be enough to simply have a reset button -- the debugger may need to 'connect under reset'.   My strong recommendation is to provide all three signals.

    Geoffrey

    v_tamakov
    v_tamakovAuthor
    Associate
    June 15, 2018
    Posted on June 15, 2018 at 12:49

    Thanks for your advice, I will follow them