Question
About stm32L stop mode uart
Posted on November 26, 2017 at 13:58
hi everyone~
Before enter stop mode ,I called HAL_UART_DeInit(&huart3) an after it was wake up from stop mode(wake up by rtc), I called HAL_UART_Init(&huart3),but after wake up uart3 can't work. What should I do?
before enter stop mode:
huart3.Instance = USART3;
if (HAL_UART_DeInit(&huart3) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }wake up from stop mode:
huart3.Instance = USART3;
huart3.Init.BaudRate = 9600; huart3.Init.WordLength = UART_WORDLENGTH_8B; huart3.Init.StopBits = UART_STOPBITS_1; huart3.Init.Parity = UART_PARITY_NONE; huart3.Init.Mode = UART_MODE_TX_RX; huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart3.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart3) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }