About Pin function
- 2 replies
- 5535 views
I would like to do UART communication using nucleo l4r5zi.
I would like to do the pin setting, but I do not know how to do that.
Please let me ask the following two questions here.
1.
Is my understanding correct that the pin settings for CN7, CN8, CN9 and CN10 of the nucleo l4r5zi have already been set and the pin settings are listed in table 11 on p36 of the manual below?
STM32-Nucleo-144-User-Manual.pdf
2.
Since the functions of CN11 and CN12 are not specifically described, is it necessary to set the pins on the microcontroller side?
If this is correct, please answer the following.
I understand that the GPIOx_AFRH and GPIOx_AFRL are used to set the pin settings.
These register specifications※ only state AF0, but do not state which function they are actually assigned to.
How is the pin setting performed?
※dm00310109-stm32l4-series-advanced-arm-based-32-bit-mcus-stmicroelectronics.pdf p347