Skip to main content
Associate II
Feb 2, 2024 4:44 AM UTC
Question

About CAN TX interrrupt (CAN_IT_TX_MAILBOX_EMPTY) is not working in the normal mode.

Hi Everyone,

                  I'm facing the issue that when i implementing the CAN interrrupt Transmit(CAN_IT_TX_MAILBOX_EMPTY) in CAN Normal mode. It going to interrupt hardfault error. But when i'm using the same concept in the loopback mode. It is working fine. so can you please provide the reason.

This topic has been closed for replies.

1 reply

mƎALLEm
ST Technical Moderator
Apr 1, 2024 3:00 PM UTC

Hello,

You need to provide more details.

If possible to share your project.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.