Skip to main content
Jwu.6
Associate
March 29, 2021
Question

Abnormal log of tfm NS interface tests with nucleo_l552ze_q board

  • March 29, 2021
  • 0 replies
  • 467 views

Hi,

When I run tfm_ns test on STM32L562E_DK discovery board:

the tf-m source code :

git clone https://git.trustedfirmware.org/TF-M/trusted-firmware-m.git

cmake .. -DTFM_PLATFORM=stm/nucleo_l552ze_q -DTFM_TOOLCHAIN_FILE=../toolchain_GNUARM.cmake -G"Unix Makefiles" -DTEST_NS=ON

the following logs are showed repeatly,I think this is abnormal. I didn't modify the source code of tf-m and tf-m-tests.

[INF] Starting bootloader

[INF] Swap type: none

[INF] Swap type: none

[INF] Bootloader chainload address offset: 0x13000

[INF] Jumping to the first image slot

[Sec Thread] func Secure image initializing!

Booting TFM func v1.2.0

Non-Secure system starting...

#### Execute test suites for the Non-secure area ####

Running Test Suite PSA protected storage NS interface tests (TFM_PS_TEST_1XXX)...

> Executing 'TFM_PS_TEST_1001'

 Description: 'Set interface'

[INF] Starting bootloader

[INF] Swap type: none

[INF] Swap type: none

[INF] Bootloader chainload address offset: 0x13000

[INF] Jumping to the first image slot

[Sec Thread] func Secure image initializing!

Booting TFM func v1.2.0

Non-Secure system starting...

#### Execute test suites for the Non-secure area ####

Running Test Suite PSA protected storage NS interface tests (TFM_PS_TEST_1XXX)...

> Executing 'TFM_PS_TEST_1001'

 Description: 'Set interface'

[INF] Starting bootloader

[INF] Swap type: none

This topic has been closed for replies.