Question
A CUBE issue: float mode from hard to ''soft'' with no explanation
Posted on July 07, 2016 at 15:04
Hi,
i have a problem with CUBE and System Workbench. Each time i click the ''Generate code'' the FPU mode in Drivers and/or Middlewares is randomly switched from hard to soft (--abi-float=soft) The code won't compile then. It's very annoying because this behavior is very random: sometimes only the Drivers branch is touched, sometimes both Drivers and Middlewares are changed. Is my problem unique or there's a solution for a ''permanent'' float setting in Eclipse? I need ''hard''. - Using the System Workshop Luna Release 2 (4.4.2) and Cube MX 4.14.0 on Windows.