Skip to main content
sholojda
Associate III
April 23, 2021
Question

8 Byte stack align in interrups (vs. 4 byte)

  • April 23, 2021
  • 10 replies
  • 4464 views

Hi. I realize this may seem simple to some of you but i realy want to undestand this as easy as it is possible.

In STM32 (for example) there is a bit called STKALIGN. If this bit is set stack is align to 8 byte instead of 4 byte.

How can i see difference in behavior when this bit is set or not? How to use this?

I know wthat align is but it is hard to undestand if i do not see how it works.

    This topic has been closed for replies.

    10 replies

    Pavel A.
    April 23, 2021

    See here to understand why it is needed:

    https://community.arm.com/developer/ip-products/processors/f/cortex-m-forum/6344/what-is-the-meaning-of-a-64-bit-aligned-stack-pointer-address

    How it works:

    Assume that interrupt strikes just after the program pushed a word on the stack, so the stack is not 8 bytes aligned.

    To align the stack for the handler, hardware automatically pushes one more word as part of "stacking" procedure, and sets bit 9 of the saved PSR to remember this.

    On exit from the handler the stack is automatically restored.

    The fine manual to read is PM0253. Enjoy ))

    --pa

    sholojda
    sholojdaAuthor
    Associate III
    April 26, 2021

    Hi.

    I read this couple of times trying to understand this. But that raised even more questions :)

    How can i see this is needed?

    How can i see this work?

    Pavel A.
    April 26, 2021

    Hmm... perhaps read it another time?

    Radosław
    Associate II
    April 27, 2021

    Probably this will be hard to obserwe. But when stack isn't 8byte aligned and in interrupt some 64-bit variable will be allocated on stack, then will be a problem. but chance for this is low and effect is unpredicted.

    Pavel A.
    April 27, 2021

    This is trivial to observe: 1.when SP is aligned on 8, push a word. Now SP is not aligned on 8. 2. Cause an interrupt, SVC for example

    --pa

    Radosław
    Associate II
    April 27, 2021

    forcing this without any efects isn't an observation.

    sholojda
    sholojdaAuthor
    Associate III
    April 27, 2021

    So Pavel i took yours clever advice, I've looked there one more time andto my surprise nothing more appeared. No more example explaining how it works. What is benefit of this 8 byte align. How can i use it.

    Tesla DeLorean
    Guru
    April 27, 2021

    It is for architectures where the data paths, busing, or memory subsystem have 64-bit paths, and where additional time penalties will occur when transactions are split.

    The ABI recommendation is for cross-platform harmony and ease of porting.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..