Skip to main content
mike louaillier
Associate III
Aug 12, 2017 1:38 AM UTC
Solved

70F6 won't start after reset

Posted on August 12, 2017 at 03:38

so i got a 70F6 uC wired up to an LED and a simple program to make it flash. i plug it into power and the program executes, but then when i hit the reset button to connect the NRST pin to ground the flashing stops and doesn't start up again. so i unplug the power and replug it in, flashing starts again.

according to the reference manual POR and NRST do essentially the same thing. NOT.

    This topic has been closed for replies.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Aug 12, 2017 2:51 AM UTC
    Posted on August 12, 2017 at 04:51

    STM32F070F6 ?

    Is the BOOT0 pin pulled to ground, or floating?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

    2 replies

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Aug 12, 2017 2:51 AM UTC
    Posted on August 12, 2017 at 04:51

    STM32F070F6 ?

    Is the BOOT0 pin pulled to ground, or floating?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    mike louaillier
    Associate III
    Aug 12, 2017 5:11 AM UTC
    Posted on August 12, 2017 at 05:11

    it's floating. i'll try tying it down....BINGO! problem solved, much obliged :)