Question
5.7'' TFT display 640X480 16bit FSMC part number
Posted on May 08, 2012 at 12:08
For my current project we are using a development board of powerAVR. It has a 3.5� TFT touchpanel with resolution 320x240, using 16bit FSMC bus for communication. But I need to have implement it on a 5.7� TFT with resolution 640x480.
We have been searching to find a suitable part which is FSMC compatible, but with no success till now. can anyone provide the details regarding the part number of the same.
The controller on the development board is STM32F103ZE and the display controller is SSD1963. It will be very appreciated if the display controller is the same.