Skip to main content
peterwrigley9
Associate II
August 13, 2008
Question

48 pin TQFP socket

Posted on August 13, 2008 at 20:34

48 pin TQFP socket

    This topic has been closed for replies.

    4 replies

    peterwrigley9
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:41

    Hi everyone,

    Does anyone have a part number for a suitable socket for development use? I have managed to track down ST's part number for the 100-pin early evaluation boards but not a suitable 48 pin variant.

    FYI Early revisions of ST's eval boards (e.g. STM3210B-EVAL) also have a /WS part number for ''with socket'' so that when the silicon is changed, the micro can be changed easily. They are very rare after product launch.

    Thanks!

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:41

    Quote:

    I think you'd be better of with one of those little TQFP-to-DIL adaptor boards from the likes of Roth, Winslow Adaptics, et al...

    For example, here's one I prepared earlier (not TQFP, but you get the idea):

    0690X00000602hfQAA.jpg0690X00000602cgQAA.jpg0690X00000602grQAA.jpg

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:41

    I think these sockets tend to be unreliable and horribly expensive.

    I think you'd be better of with one of those little TQFP-to-DIL adaptor boards from the likes of Roth, Winslow Adaptics, et al...

    jj_it
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:41

    Perhaps this will work - to our joint benefit.

    My (usa) firm is building small pcbs holding STM32 (48,64 or 100 pin QFPs) small xtal, VReg, Caps, SOT Uart Level Shifter, and hi-capacity, 8 pin soic, spi eeprom. Mini JTAG and I/O connector - with optional 0.1'' adapter pcbs. Plan now is to build about 50 ea for our internal needs - can build more if the forum requests... Small qty. price is about cost of micro + 23 USD, fob usa - assembled/tested.

    This functional board should be less expensive than the mechanical, clamp connector you described...