Skip to main content
Associate III
January 16, 2026
Question

4 x 4 keypad with Nucleo 411RE and HAL

I created standard project in CubeIDE for Nucleo 411RE ( with default settings)
I found some code (which interfaces 4x4 keypad) and try to repeat it with HAL
I setup pins PC0,PC1,PC2,PC3 with Input mode and Pull-up.

PC4,PC5,PC6,PC7 as Output and GPIO output level - High 
all this based on my understanding code I try to repeat ( below )

Did I do correct repeating with HAL ? ( As I understand CubeIDE will generate GPIOs the same way as function ?

void keypad_init(void)
{

	/*Enable clock access to GPIOC*/
	RCC->AHB1ENR|=RCC_AHB1ENR_GPIOCEN;

	/*Set PC0 to PC3 as input*/
	GPIOC->MODER &= ~(GPIO_MODER_MODE0|GPIO_MODER_MODE1|GPIO_MODER_MODE2|GPIO_MODER_MODE3);

	/* Activate internal pullup resistor for PC0 to PC3*/
	GPIOC->PUPDR|=GPIO_PUPDR_PUPD0_0|GPIO_PUPDR_PUPD1_0|GPIO_PUPDR_PUPD2_0|GPIO_PUPDR_PUPD3_0;

	/*Set PC4 to PC7 as output*/
	GPIOC->MODER |= GPIO_MODER_MODE4_0|GPIO_MODER_MODE5_0|GPIO_MODER_MODE6_0|GPIO_MODER_MODE7_0;

	GPIOC->MODER &=~( GPIO_MODER_MODE4_1|GPIO_MODER_MODE5_1|GPIO_MODER_MODE6_1|GPIO_MODER_MODE7_1);

	/*Set PC4 to PC7 as high*/

	GPIOC->BSRR = GPIO_BSRR_BS4|GPIO_BSRR_BS5|GPIO_BSRR_BS6|GPIO_BSRR_BS7;
}

2 replies

Pavel A.
January 17, 2026

> Did I do correct repeating with HAL ?

Your code is not "HAL". It only uses symbols defined in the ST device .h file for the STM32F4 - which is good because helps others understand the code. But it does not use any HAL or "LL" functions.

> As I understand CubeIDE will generate GPIOs the same way as function

No, it calls a HAL function rather than set GPIO registers directly.

By the way, CubeIDE does not generate code any longer. This function has moved to CubeMX.

 

gbm
Super User
January 17, 2026

For simple matrix scanning, set all pins (rows and columns) as open-drain outputs with pull-ups. Set all row pins low, column pins high.

Then you need to implement a simple state machine in timer interrupt with three states:

DetectColumn (initial state): if any column input low - store column number, set that column state to low and all the other lines to high, switch state to CheckRow.

CheckRow: read row input state, deactivate all columns, activate all rows; if any row input was low, store row number, determine key pressed, switch to WaitForRelease; otherwise switch to DetectColumn.

WaitForRelease: if all column inputs high, switch to DetectColumn.

The state machine processing should be called every 5..10 ms.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice