Skip to main content
csdominik
Associate II
November 14, 2011
Question

4 Input PWM and 4 output PWM

  • November 14, 2011
  • 2 replies
  • 786 views
Posted on November 14, 2011 at 01:36

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    November 14, 2011
    Posted on November 14, 2011 at 03:28

          TIM_TimeBaseStructure.TIM_Prescaler = 1440 - 1;  // 72MHz/1440 = 50kHz

          TIM_TimeBaseStructure.TIM_Period = 1000 - 1; // 50KHz/1000 = 50 Hz

          TIM_TimeBaseStructure.TIM_ClockDivision = 0;

          TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

          TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);

    Then you can program the width between 0-1000 (20 us units), and the output frequency of PWM CH1-4 will be 50 Hz

    You could used 144-1 and 10000-1, or 36-1 and 40000-1, if you need more fine grain control of the width.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    csdominik
    csdominikAuthor
    Associate II
    November 16, 2011
    Posted on November 16, 2011 at 13:36

    Thank you for suggestion about prescaler and period.

    Due to problems with EXTI and STM32F1 I have decided to try STM32F4 uC  with have many more timers.

    If someone have any solution orr suggestion for my problem with EXTI interrupts, please send me reply.