Skip to main content
stanzanim
Associate III
January 8, 2016
Question

32 sum with saturation

Posted on January 08, 2016 at 18:25

hello forum

I am using a Cortex M0+ and I am looking for suggestions about handling saturation with 32 bit addition.I found this code in the web 

uint32_t sadd32(uint32_t a, uint32_t b)

{ return (a > (1<<32-1) - b) ? ((1<<32)-1) : a + b;}

which can probably  extended to int32_t (which puzzles me :) ). I am looking for possible suggestions about more efficient assembly implementation

thanks
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    January 8, 2016
    Posted on January 08, 2016 at 19:32

    PRESERVE8
    THUMB
    AREA |.text|, CODE, READONLY
    ; M0 version
    AddSatU32 PROC
    EXPORT AddSatU32
    ; Entry
    ; R0 = A (uint32_t)
    ; R1 = B (uint32_t)
    ; Exit
    ; R0 = A+B, or 0xFFFFFFFF
    add r0, r0, r1 ; do the sum
    sbcs r1, r1, r1 ; propagate carry 1->0x00000000, 0->0xFFFFFFFF
    mvns r1, r1 ; not
    orrs r0, r1 ; or (add's carry forces OR with 0xFFFFFFFF)
    bx lr
    ENDP ; AddSatU32 - sourcer32@gmail.com
    END

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    stanzanim
    stanzanimAuthor
    Associate III
    January 12, 2016
    Posted on January 12, 2016 at 11:27

    thank much clive for your quick reply!

    what about signed sum? it should be enough to check the V flag right? if you have a debugged example with signed operands please post it