3-wire 9-bit SPI using STM32F030C6
I need to interface ILE9341V TFT display with STM32F030C6 MCU.
My project hardware has only 3 wires (CSX, SDA and SCL) from the display side.
By referring the TFT display's datasheet, I found that I have to use 3-wire 9-bit mode only (to be compatible with the hardware).
Am I correct here ?
If so, I would like to know how to send 9 bits (1 D/C bit + 8 data bits) using SPI APIs.
I have gone through many blogs and forums on internet for the same but ended up with the option 'Bit-banding SPI'.
But I think it will consume more power and will take long time.
Also, I am afraid that handling other interrupt while using 'Bit-banding/software SPI' may end up in misbehavior of the TFT display.
Seeking for your support here.