Skip to main content
sol barnett
Associate II
June 3, 2018
Question

14 bit DCMI with Boson camera

Posted on June 03, 2018 at 21:30

Hi I am using the DCMI on STM32H743 in 14 bit mode  with a 16 bit camera but I am only use the 14bits MSB  but I only get 8 bit through the system .

if I change to 12 or 10 the same again only the first 8 bits but a images comes through . but if I select 8 bit mode I get 4 images .

can anyone help ? has anyone used the H743 with 14 bit DCMI ?

thanks 

Sol

    This topic has been closed for replies.

    6 replies

    ST Technical Moderator
    June 4, 2018
    Posted on June 04, 2018 at 11:48

    Hello

    sol.barnett

    ,

    What do you mean'but I only get 8 bit through the system' ? How do you get 8 bit ?

    Which data format used:

    RGB, JPEG, YUV...?

    It seems to me that you have a configuration problem.

    Make sure toconfigure properly your DCMI and camera module,based on the

    DCMI application note

    http://www.st.com/content/ccc/resource/technical/document/application_note/group0/c0/ef/15/38/d1/d6/49/88/DM00373474/files/DM003734pdf/jcr:content/translations/en.DM003734pdf

    which contains DCMI use case examples and DCMI examples based on STM32CubeMX.

    With Regards,

    Imen.

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    sol barnett
    Associate II
    June 4, 2018
    Posted on June 04, 2018 at 11:56

    Hi Imen 

    I can send you the set up code could you look at it for me ?

      

    Thanks

    Sol

    sol barnett
    Associate II
    June 4, 2018
    Posted on June 04, 2018 at 12:19

    /* DCMI init function */

    static void MX_DCMI_Init(void)

    {

    hdcmi.Instance = DCMI;

    hdcmi.Init.SynchroMode = DCMI_SYNCHRO_HARDWARE;

    hdcmi.Init.PCKPolarity = DCMI_PCKPOLARITY_RISING; //ini

    //hdcmi.Init.PCKPolarity = DCMI_PCKPOLARITY_FALLING; //works the same pic

    hdcmi.Init.VSPolarity = DCMI_VSPOLARITY_LOW;//ini

    //hdcmi.Init.VSPolarity = DCMI_VSPOLARITY_HIGH; // no pic

    hdcmi.Init.HSPolarity = DCMI_HSPOLARITY_LOW;// ini

    //hdcmi.Init.HSPolarity = DCMI_HSPOLARITY_HIGH;// no pic

    hdcmi.Init.CaptureRate = DCMI_CR_ALL_FRAME; //ini was

    //hdcmi.Init.CaptureRate = DCMI_CR_ALTERNATE_2_FRAME;

    hdcmi.Init.ExtendedDataMode = DCMI_EXTEND_DATA_14B;//CHANGED TO 12 NO DIFFERENCE, 8 bit - got 4 small pics

    hdcmi.Init.JPEGMode = DCMI_JPEG_DISABLE;

    hdcmi.Init.ByteSelectMode = DCMI_BSM_ALL;

    hdcmi.Init.ByteSelectStart = DCMI_OEBS_ODD;

    hdcmi.Init.LineSelectMode = DCMI_LSM_ALL;

    hdcmi.Init.LineSelectStart = DCMI_OELS_ODD;

    if (HAL_DCMI_Init(&hdcmi) != HAL_OK)

    {

    _Error_Handler(__FILE__, __LINE__);

    }

    }

    /**

    * Enable DMA controller clock

    */

    static void MX_DMA_Init(void)

    {

    /* DMA controller clock enable */

    __HAL_RCC_DMA1_CLK_ENABLE();

    /* DMA interrupt init */

    /* DMA1_Stream0_IRQn interrupt configuration */

    HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0x0F, 0); //DCMI

    HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn);

    }

    void BSP_CAMERA_SnapshotStart(uint32_t *buff)

    {

    /* Start the camera capture */

    HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_CONTINUOUS, (uint32_t)buff, CAM_FRAME_BUFFER_SIZE / 2);

    }

    void DMA1_Stream0_IRQHandler_complete() //DCMI

    {

    if(bFrameEthUnload2)

    {

    bFrameEthLoad2 = true;

    bFrameEthUnload2 = false;

    memcpy((uint16_t *)cam_frame_buffer_2, (uint16_t *)cam_frame_buffer_1, sizeof(cam_frame_buffer_1));

    bFrameReady = true;

    cnt_frames_written2++;

    }

    else if(bFrameEthUnload3)

    {

    bFrameEthLoad3 = true;

    bFrameEthUnload3 = false;

    memcpy((uint16_t *)cam_frame_buffer_3, (uint16_t *)cam_frame_buffer_1, sizeof(cam_frame_buffer_1));

    bFrameReady = true;

    cnt_frames_written3++;

    }

    }

    void HAL_DCMI_MspInit(DCMI_HandleTypeDef* hdcmi)

    {

    GPIO_InitTypeDef GPIO_InitStruct;

    if(hdcmi->Instance==DCMI)

    {

    /* USER CODE BEGIN DCMI_MspInit 0 */

    /* USER CODE END DCMI_MspInit 0 */

    /* Peripheral clock enable */

    __HAL_RCC_DCMI_CLK_ENABLE();

    /**DCMI GPIO Configuration

    PE4 ------> DCMI_D4

    PE5 ------> DCMI_D6

    PE6 ------> DCMI_D7

    PF10 ------> DCMI_D11

    PA4 ------> DCMI_HSYNC

    PA6 ------> DCMI_PIXCLK

    PF11 ------> DCMI_D12

    PG7 ------> DCMI_D13

    PC8 ------> DCMI_D2

    PC9 ------> DCMI_D3

    PA9 ------> DCMI_D0

    PA10 ------> DCMI_D1

    PC10 ------> DCMI_D8

    PC12 ------> DCMI_D9

    PD3 ------> DCMI_D5

    PG9 ------> DCMI_VSYNC

    PB5 ------> DCMI_D10

    */

    GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6;

    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

    GPIO_InitStruct.Pull = GPIO_NOPULL;

    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

    GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;

    HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

    GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11;

    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

    GPIO_InitStruct.Pull = GPIO_NOPULL;

    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

    GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;

    HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);

    GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_6|GPIO_PIN_9|GPIO_PIN_10;

    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

    GPIO_InitStruct.Pull = GPIO_NOPULL;

    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

    GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;

    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

    GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_9;

    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

    GPIO_InitStruct.Pull = GPIO_NOPULL;

    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

    GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;

    HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

    GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10|GPIO_PIN_12;

    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

    GPIO_InitStruct.Pull = GPIO_NOPULL;

    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

    GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;

    HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

    GPIO_InitStruct.Pin = GPIO_PIN_3;

    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

    GPIO_InitStruct.Pull = GPIO_NOPULL;

    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

    GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;

    HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

    GPIO_InitStruct.Pin = GPIO_PIN_5;

    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

    GPIO_InitStruct.Pull = GPIO_NOPULL;

    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

    GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;

    HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

    /* DCMI DMA Init */

    /* DCMI Init */

    hdma_dcmi.Instance = DMA1_Stream0;

    hdma_dcmi.Init.Request = DMA_REQUEST_DCMI;

    hdma_dcmi.Init.Direction = DMA_PERIPH_TO_MEMORY;

    hdma_dcmi.Init.PeriphInc = DMA_PINC_DISABLE;

    hdma_dcmi.Init.MemInc = DMA_MINC_ENABLE;

    hdma_dcmi.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;

    hdma_dcmi.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;

    hdma_dcmi.Init.Mode = DMA_CIRCULAR; //

    hdma_dcmi.Init.Priority = DMA_PRIORITY_HIGH;

    hdma_dcmi.Init.FIFOMode = DMA_FIFOMODE_ENABLE;

    hdma_dcmi.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;

    hdma_dcmi.Init.MemBurst = DMA_MBURST_SINGLE;

    hdma_dcmi.Init.PeriphBurst = DMA_PBURST_SINGLE;

    if (HAL_DMA_Init(&hdma_dcmi) != HAL_OK)

    {

    _Error_Handler(__FILE__, __LINE__);

    }

    __HAL_LINKDMA(hdcmi,DMA_Handle,hdma_dcmi);

    /* USER CODE BEGIN DCMI_MspInit 1 */

    /* USER CODE END DCMI_MspInit 1 */

    }

    }

    Tesla DeLorean
    Guru
    June 4, 2018
    Posted on June 04, 2018 at 13:42

    The 14-bit wide allows for cameras of that bit depth to connect with higher bandwidth, but most have byte packing methods or formatting. As Imen indicates the JPEG modes typically use this too, but the byte streams also pack in memory much more efficiently as the image size scales.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    sol barnett
    Associate II
    June 4, 2018
    Posted on June 04, 2018 at 13:52

    not sure if this is the Case with the Boson Camera  by Flir  .  I tested the DCMI interface  by removing one bit at a time .

    when I get to bit 8 I no longer get any data come through . I have also checked bit 8 onwards of the camera by putting it in the first 8 bits of the DCMI . so the problem is there is no bits ether collected after bit 7 or the data is going somewhere  else ?

    Tesla DeLorean
    Guru
    June 4, 2018
    Posted on June 04, 2018 at 16:15

    Not a camera I've used, or reviewed the documentation for.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..