Skip to main content
dimax
Associate III
November 23, 2012
Question

100pin device FSMC and Graphic LCD

  • November 23, 2012
  • 2 replies
  • 615 views
Posted on November 23, 2012 at 12:12

HI,

I'm I right to assume that in 100pin devices FSMC can be used only in multiplexed mode as Address bus is not available on this chips?

Or one should drive Address lines in FW. So that A0 used as RS signal for Graphic LCD connection should be toggled in FW as regular non alternate function GPIO while rest of the transaction can be done by FSMC?

    This topic has been closed for replies.

    2 replies

    waclawek.jan
    Super User
    November 23, 2012
    Posted on November 23, 2012 at 16:58

    If I understand correctly, you need only one arbitrary address line. I'd say you still could use the high (A16 and up) addresses, which are mapped out on the 100-pin packages pins.

    JW
    dimax
    dimaxAuthor
    Associate III
    November 23, 2012
    Posted on November 23, 2012 at 20:13

    Good Idea, did not think about it.

    Yes it should be OK in this case and even better then using A0 as in this case I can make 32bit access (that will be spitted into two 16bit transfers or 4 8-bit transfers depending of selected data bus width) without care of A0 get changed.