Skip to main content
Senior
Jan 14, 2026 11:20 PM UTC
Question

100% compatible STM32C031G6U6 drop-in replacement

Hi,

is there a 64Kb drop-in replacement for the STM32C031G6U6 (which is only 32kb)?

We need to find a part where - ideally - we just use the same code without any mods, this is the most important part.

And is there perhaps a tool that helps with that? Or at least allows us to make an accurate comparison check between two parts?

We just use GPIOs and 1 x RS232 and 1 x I2C in their default pin locations.

Thank you

3 replies

TDK
Jan 14, 2026 11:39 PM UTC

The STM32C031 is only available in 16 kB or 32 kB flash sizes.

TDK_0-1768433793473.png

 

The part selector in STM32CubeMX can help you narrow down and find a suitable chip. Here are STM32C0 chips with 64+ kB of flash.

TDK_1-1768433914396.png

 

Ultimately it depends on what your program does, but in most cases those will be able to run the same code without modification.

"If you feel a post has answered your question, please click ""Accept as Solution""."
gbm
Super User
Jan 15, 2026 7:07 AM UTC

How about C071?

Maybe changing the compiler optimization level from the default -O0 to -Os will be enough to solve your problem without changing the chip. If not, get rid of HAL. ;)

 

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Simon.T
ST Employee
Jan 15, 2026 8:40 AM UTC

Hello @Ricko ,

 

The  STM32C051G8U6 is the 64kB flash drop in replacement of STM32C031G6U6.

They are in the same series, so the package pinout, alternate function and platform are the same. The main differences are that in STM32C051G8U6  there are more flash and more peripherals.

 

You can have a look on this application where STM32G0 and STM32C0 are compared. There are multiple tables comparing the devices; https://www.st.com/resource/en/application_note/an5969-migrating-between-stm32g0-and-stm32c0-mcus-stmicroelectronics.pdf

 

Best regards,

 

Simon