Skip to main content
alexanderpolleti9
Associate II
March 3, 2016
Question

1 second missing at reading RTC on STM32L151

  • March 3, 2016
  • 0 replies
  • 463 views
Posted on March 03, 2016 at 17:09

Hello everyone,

I am using the RTC on a stm32l151VC. I am using sleep modes in order so save battery life. As I need to tell the OS how long I have been sleeping (Systick is turned off) I save the time tick before I start sleeping and one after I was sleeping. As I never sleep more than 1 second I just use the seconds and subsecond from rtc:


uint32_t DT_GetRtcMsTick(
void
)

{

uint32_t result;


/* To ensure consistency between the 3 values, reading either RTC_SSR or

RTC_TR locks the values in the higher-order calendar shadow registers

until RTC_DR is read. */

__disable_irq();

HAL_RTC_WaitForSynchro(&hrtc);

uint32_t subSeconds = hrtc.Instance->SSR;

uint32_t timeReg = hrtc.Instance->TR;

uint32_t date = (uint32_t)hrtc.Instance->DR;

(
void
)date;

__enable_irq();


subSeconds &= RTC_SSR_SS;

timeReg &= RTC_TR_RESERVED_MASK;


/* Second fraction = ( PREDIV_S - SS ) / ( PREDIV_S + 1 )

PEDIV_S = 255 */

/* in ms, so x1000 */

result = ((DT_PREDIV_S - subSeconds) * 1000) / (DT_PREDIV_S + 1);

result += RTC_Bcd2ToByte(timeReg & (RTC_TR_ST | RTC_TR_SU)) * 1000;

return
result;

}

It seems like sometimes there is 1 second (1000ms) missing from either start or end. Any ideas where this could come from? Alexander #stm32-stm32l151-rtc
This topic has been closed for replies.