Skip to main content
Wlie
Visitor II
April 2, 2021
Question

デ�?ッガー�?�らMCU�?�プログラムを書�??込む際�?��?プログラム�?�書�??込�?�自体�?��?ェック(MCU�?�書�??込ん�?�プログラム�?�間�?��?��?��?��?��?��?�確�?�?�るよ�?��?�処�?�)�?�入�?��?��?�る�?��?��?�ょ�?��?�?

  • April 2, 2021
  • 1 reply
  • 441 views

..

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    April 2, 2021

    When writing a program from the debugger to the MCU, is there a check (a process to confirm that the program written to the MCU is correct) in the program writing itself?

    In things like Keil there is a debugger/flasher option to "Verify After Download"

    You can also have a post-link step/method to add a checksum or CRC to the firmware image that the code in the firmware itself can subsequently recompute and validate.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..