Skip to main content
Associate III
Jan 13, 2026 12:25 AM UTC
Solved

X-NUCLEO-IHM16M1 Max Current

I am currently using the X‑NUCLEO‑IHM16M1 expansion board and noticed a discrepancy between the Motor Control Workbench and the official ST documentation regarding the rated current.

  • In Motor Control Workbench, the Rated Current is shown as 2.1 A.
  • On the official product page and data brief, it states Output current up to 1.5 A rms

https://www.st.com/en/evaluation-tools/p-nucleo-ihm03.html

 

Could you please clarify the following:

  1. What is the basis for the 2.1 A figure shown in Motor Control Workbench (e.g., RMS, peak, or internal limit)?
  2. Which current rating should be considered as the actual board limit for design purposes?
  3. Does the difference relate to the STSPIN830 driver’s internal specifications or to a configuration setting in the tool?

Thank you very much for your support.

Best regards,

HyeonSeok​

STuser2Best answer
Senior III
Jan 13, 2026 3:19 AM UTC

Check the below thread

Solved: Application Current and Over Current Protection Pa... - STMicroelectronics Community

My understanding is 

1.5A is RMS value 

1.5* Sqrt(2) = 2.12 A

 

1 reply

STuser2Best answer
Senior III
Jan 13, 2026 3:19 AM UTC

Check the below thread

Solved: Application Current and Over Current Protection Pa... - STMicroelectronics Community

My understanding is 

1.5A is RMS value 

1.5* Sqrt(2) = 2.12 A