Visitor II
October 15, 2019
Question
X-NUCLEO IHM07M1 - Motor Profiler Problem
- 3 replies
- 2545 views
I bought a F401RE and an IHM07M1 to work on the subject BLDC a couple of weeks ago but, I could not profile the motor.
My motor is T-Motor U8 170kw. It has 36 coils and 42 poles. I connected my boards successfully but, when I clicked "Start Profile" it gives me the error message "The measurement is taking too time" and after clicking "continue anyway" the motor doesn't run.
I attached my setup, motor and the warning message.
I would be really happy if someone could help me.
Thanks!