Skip to main content
jerry2
Associate III
May 27, 2022
Question

X-NUCLEO-IHM07M1 Motor Driver Board

The Quick Start Guide for this board implies it is compatible only with the following Nucleo boards:

NUCLEO-F030R8

NUCLEO-F103RB

NUCLEO-F302R8

NUCLEO-F401RE

Does anyone know if it will work with any of the Nucleo F7 or H7 boards?

This topic has been closed for replies.

1 reply

ST Technical Moderator
May 29, 2022

Hello @jerry2​ ,

The X-NUCLEO-IHM07M1 is compatible with STM32 Nucleo boards, with the ST Morpho connector and supports the addition of other boards which can be stacked with onto a single STM32 Nucleo board.

Firstly, you should check if your board is pin to pin compatible with the headers, check the GPIO to enable the motor controller board.

You can adapt the available example (Eg: for NUCLEO-F401RE) to your board.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks