Skip to main content
akara.31
Visitor II
June 18, 2023
Solved

X-NUCLEO-IHM01A1 and development board

Hi STM,

I am having NUCLEO-476RG and I am planning project with steppers (by using X-NUCLEO-IHM01A1). Can I connect this expansion with my development board. And also, what is the maximum number of expansion boards I can connect to the development board. I am asking that as my project should use 7 motors?

Regards,

Aleksandar

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    June 27, 2023

    Yes, in principle you can also operate the X-NUCLEO-IHM01A1 with the NUCLEO-L476RG. It would make sense to use the software package X-CUBE-SPN1, because you can start immediately with it. It doesn't contain a finished project for STM32L476, but the libraries are already included for STM32L4, so they can be adapted relatively quickly.

    Regarding the second question about the number of expansion boards: a maximum of 3 boards per SPI channel can be controlled in daisy chain. Theoretically, you could also connect more X-NUCLEO-IHM01A1, but this would require more extensive reconfigurations in order to control the additional boards via a second and third SPI port of the STM32L476.

    Does it help?

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    2 replies

    ST Employee
    June 27, 2023

    Hello, the MCSDK only supports FOC and 6-Steps algorithms.
    The stepper is therefore not supported on MCSDK but you can find more information on this page about the steppers:
    https://www.st.com/en/applications/industrial-motor-control/stepper-motor-control.html#overview
    Therefore the NUCLEO-L476RG board can be used on MCSDK to the motor control for FOC or 6-Steps algorithmes.
    And we will soon be able to have dual motor control with a single board on the next release.

    "If you agree with my answer, please accept it by clicking on ""Accept as solution""."
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    June 27, 2023

    Yes, in principle you can also operate the X-NUCLEO-IHM01A1 with the NUCLEO-L476RG. It would make sense to use the software package X-CUBE-SPN1, because you can start immediately with it. It doesn't contain a finished project for STM32L476, but the libraries are already included for STM32L4, so they can be adapted relatively quickly.

    Regarding the second question about the number of expansion boards: a maximum of 3 boards per SPI channel can be controlled in daisy chain. Theoretically, you could also connect more X-NUCLEO-IHM01A1, but this would require more extensive reconfigurations in order to control the additional boards via a second and third SPI port of the STM32L476.

    Does it help?

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.